Search term

Schaeffler at the AMB 2022, Hall C2, Booth E21 Schaeffler supplements bearing portfolio with angular measuring system for high speed rotary tables

Pressrelease Stage Image
ZKLDF-series bearings are now available with incremental angular measuring system, ordering designation: ZKLDFMI

2022-09-13 | Schweinfurt/Stuttgart

  • Incremental angular measuring system now optionally available for ZKLDF-series axial angular contact ball bearings
  • Angular measuring system integrated into the rotary table bearing support offers very high accuracy and extremely easy mounting
  • No restrictions on the hollow shaft diameter even with measuring system

Schaeffler is presenting its ZKLDF-series axial angular contact ball bearings with an optional integral, incremental angular measuring system (ZKLDFMI) at the AMB 2022 in Stuttgart. Due to their suitability for very high speeds, low breakaway torque, and low friction levels, ZKLDF-type bearings are preferably used in high speed machine tools for machining non-ferrous metals, plastics, and wood. Highly dynamic rotary indexing tables in industrial automation are also a preferred area of application. Because ZKLDF bearings in rotary axes are almost always combined with direct drives, the integration of an angular measuring system was a logical step. As with all the other angular measuring systems from Schaeffler for the machine tool sector, an inductive AMOSIN® angular measuring system is also used in ZKLDFMI bearings.

A bearing-integrated solution with multiple benefits
The dimensional scale of AMOSIN® angular measuring systems is affixed to the precision ground and perfectly true-running bearing inner ring. The greatest possible measurement accuracy is achieved by positioning the measuring system in the bearing plane. The measuring head is screw mounted directly to the stationary bearing outer ring. The inductive measuring system is particularly resistant to lubricants and magnetic fields. The maximum speed of the ZKLDF bearing can be fully utilized due to the high output frequency of the incremental measuring head. The central passage is not influenced by the measuring system, which ensures design freedom for the media feed-throughs.

The incremental system has distance-coded reference marks. Thus, although the controller needs to do a reference run when first switched on, the run is very brief, as the scanner only needs to pass over the two reference marks. Once the reference run is complete, the absolute angle position is known and machining can commence.

Publisher: Schaeffler AG
Country: Germany

Related media

Terms of use for Schaeffler press pictures

Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.

We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.

Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.

Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany

presse@schaeffler.com

Downloads

Package (Press release + media)

Share Page

Schaeffler applies cookies to secure an optimal use. With the further use of this website you accept the application of cookies. More Information

Accept