Schaeffler is the official innovation partner of the DTM
Power and outstanding performance, thrilling action on the track, and cutting-edge internal combustion engine technology – that is the DTM. Since 1984, this racing series has been attracting fans with a combination of enthralling motor sport and a colorful program of entertainment with additional high-level racing series that are held during the race weekends.
Brand ambassador Marco Wittmann has been competing in the DTM in the green Schaeffler BMW since 2019. 2026 sees the two-time champion with the #11 car take on his fourteenth season, in which Schaeffler and the Green Machine will play the important role off innovation partner to the popular racing series. The company is actively leveraging its technological expertise to lead the racing series into an attractive future. The Schaeffler Innovation Taxi Audi R8 LMS GT2, which will again feature at every DTM race weekend in the 2026 season with Markus Winkelhock at the wheel, is a clear commitment to this objective.
A pioneer in the DTM
Schaeffler has been actively involved in the DTM for many years and has been supporting drivers and teams with its expertise in motor sport and technology:
- 2011
Schaeffler lends its name to the Schaeffler Audi and secures the DTM drivers’ title in its first year with Martin Tomczyk - 2012/13
Mike Rockenfeller becomes Schaeffler’s new DTM driver and wins the DTM drivers’ title in the second year of the partnership - 2019
Start of the premium partnership with BMW M Motorsport with Marco Wittmann at the wheel - 2023
The Audi R8 LMS GT2 DTM Innovation Taxi, with Schaeffler technology on board, celebrates its debut - 2026
Car #11 is ready for the new season: the Schaeffler BMW M4 GT3 EVO with Schaeffler brand ambassador Marco Wittmann at the wheel
Schaeffler makes technology tangible
As official innovation partner, Schaeffler will once again play an important role in the DTM in 2026. The company has always stood for technological progress. Motorsport is often used as a development lab for technologies that make their way from the racetrack to the road, and thereby into series production.
The Schaeffler innovation taxi, driven by brand ambassador Markus Winkelhock, is a good example of this. As a carrier vehicle for innovative technical ideas and their implementation, it showcases technological advances to the public at racing speed and generates enthusiasm with driving experiences. Throughout the season, Schaeffler will be deploying cutting-edge technologies in the Audi R8 LMS GT2 – which, from 2026, will be clearly recognisable in its green and white livery – offering a glimpse into the future of mobility.
On the racetrack, the partnership between Schaeffler and Marco Wittmann is entering its eighth year in 2026. The Green Machine, Wittmann’s BMW M4 GT3 EVO, is once again painted in the typical Schaeffler green, making it easily identifiable in the field. Like last year, the Schaeffler brand ambassador and two-time DTM champion will be representing Schubert Motorsport, who claimed the DTM Team title in 2022 and 2024.
Marco Wittmann and his Green Machine
Marco Wittmann and Schaeffler will enter the eighth year of their partnership in 2026. Wittmann – a dyed-in-the-wool Franconian who grew up and still lives just a short distance from Schaeffler’s headquarters in Herzogenaurach – has now become a part of the Schaeffler family without whom it would no longer be complete. He has already brought home the DTM drivers’ title twice, which currently makes him one of the DTM’s most successful and experienced drivers.
Marco Wittmann makes regular visits to Schaeffler’s headquarters. “The partnership with a regional partner like Schaeffler is something special. Thanks to the close proximity to my home, we can regularly meet for a face-to-face talk in Herzogenaurach”, says Wittmann who is clearly delighted with the collaboration.
The Green Machine: Schaeffler BMW M4 GT3 EVO
For the BMW M Motorsport engineers, the key to optimising the BMW M4 GT3 was intense dialogue with the teams and drivers. In the case of the BMW M4 GT3 EVO, the focus was on handling, efficiency and reliability. Of course, Schaeffler technologies are also on board: these include a clutch actuator, a valve train with camshaft adjustment and a high-pressure fuel pump drive, as well as a throttle valve and a tensioner pulley in the belt drive.
- Capacity: 2,993 cm3
- Straight-six with M TwinPower Turbo technology
- Cylinders: 6
- Output: up to 590 hp
- Specific output: approx. 197 hp/l
- Dimensions: 5,020 mm/ 2,040 mm/ 1,308 mm (L/B/H)
Schaeffler technologies for the DTM
If it says Schaeffler on the outside, it's Schaeffler on the inside: find out which Schaeffler technologies power Marco Wittmann's Green Machine.
- Hydraulic Lash Adjuster
Installed on the inlet and outlet side of the valve train, it serves to compensate for valve clearance. - ETC – Electronic Throttle Control
In the intake tract, the ETC precisely regulates the air supply to the engine and enables dynamic adjustment of the air flow depending on driving conditions, load requirements and control strategy. - MCA – Modular Clutch Actuator
Operates the clutch without any mechanical or hydraulic connection to the pedal. The clutch-by-wire system is used in the DTM as a start-up clutch - Roller tappets for high-pressure petrol pumps
In the cylinder head of the combustion engine, roller tappets drive the high-pressure pump for direct injection. - Finger Follower
It ensures the required valve lift on the inlet and outlet sides of the valve train.