Search term

Schaeffler at EMO 2025 (Hall 6, Booth I46) New series for automation: Four-row linear recirculating ball bearing and guideway assembly in X arrangement

The standout features of Schaeffler’s KLLT four-row linear recirculating ball bearing and guideway assembly are the X arrangement of the raceways and an optimized lubrication and sealing system. Image: Schaeffler
The standout features of Schaeffler’s KLLT four-row linear recirculating ball bearing and guideway assembly are the X arrangement of the raceways and an optimized lubrication and sealing system. This product complements Schaeffler’s range of monorail guidance systems, consisting of KUVE-B four-row monorail guidance systems (O arrangement), six-row KUSE-XL monorail guidance systems, RUE-F linear recirculating roller bearing and guideway assemblies, and KUEM-E two-row miniature recirculating ball bearing and guideway assemblies. Image: Schaeffler

2025-09-10 | Schweinfurt

  • New KLLT four-row linear recirculating ball bearing and guideway assembly is ideal for a wide range of handling axes
  • New series can deal with larger tolerances in the mounting geometry
  • Maximum flexibility thanks to eight different carriages

As the inventor of the rolling element linear guidance system, the Motion Technology Company Schaeffler has decisively shaped the development of monorail guidance systems for more than 50 years and is one of the world’s leading vendors in this field. For the rapidly growing automation market surrounding machine tools – with its numerous handling systems – as well as for additive manufacturing machines and many other applications, Schaeffler will present its new KLLT four-row linear recirculating bearing and guideway assembly in X arrangement at EMO 2025.

The all-rounder among four-row linear recirculating ball bearing and guideway systems
In terms of design, the standout features of the new variant are the X arrangement of the raceways and an improved lubrication and sealing system. In conjunction with a robust structure, the new KLLT series performs the job of an “all-round linear recirculating bearing and guideway assembly” for applications with larger tolerances in the mounting geometry. Eight different carriages (KWLT) – in long, short, high and low versions, and with and without flange – offer maximum design scope and flexibility. All carriages are interchangeable within ISO 12090-1. A lubricant reservoir has been integrated into the end pieces to allow especially long re-lubrication intervals. The arrangement of the raceways in a 45° angle ensures uniform load distribution, load-bearing capacity and rigidity in all four main load directions, and as a result provides great design flexibility.

Tolerant of adjacent structures with geometrical deviations
Unlike the particularly rigid KUVE-B four-row recirculating ball bearing and guideway assemblies in O arrangement, the new KLLT recirculating ball bearing and guideway assemblies are in an X arrangement. In combination with the larger rolling elements and the resulting lower rigidity, the KLLT recirculating ball bearing and guideway assemblies can better compensate for larger tolerances in the adjacent geometry. When mounted, this results in lower reactive forces. This makes the KLLT ideal for handling when using drawn structural profiles in aluminum or welded structures with higher tolerances.

Easy to install and inexpensive spare parts inventory
The KLLT four-row linear recirculating ball bearing and guideway assemblies are available in six sizes: 15, 20, 25, 30, 35, 45. For all sizes, the maximum length of the monorails is around 4,000 millimeters. Longer monorails are put together from several sections. The patented plastic caps KA-TN/B allow efficient closure of the mounting holes in the guide rails. The necessary number are enclosed loose with every standard TKLT rail.

Publisher: Schaeffler Technologies AG & Co. KG, Schweinfurt
Country: Germany

Related media

Terms of use for Schaeffler press pictures

Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.

We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.

Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.

Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany

presse@schaeffler.com

Downloads

Package (Press release + media)

Share Page

Schaeffler applies cookies to secure an optimal use. With the further use of this website you accept the application of cookies. More Information

Accept