Schaeffler at bauma 2025 (Hall 6, Booth 103) Schaeffler presents complete range of Ewellix electromechanical linear actuators
2025-04-03 | Schweinfurt
- Ewellix electromechanical linear actuators offer outstanding controllability and efficiency
 - Large range of sizes, spindle drives, and motor-gear configurations
 - Efficient adjustment solutions for construction machinery
 
The electrification of construction machinery is a strategic objective of the sector that has made significant progress in recent years. Development efforts are currently focusing on highly efficient electric drive systems and electromechanical actuators. For this market, Motion Technology Company Schaeffler offers a wide range of Ewellix electromechanical linear actuators.
The actuators CAHB10 and CAHB2x, with rated forces of up to 10 kN, were specifically developed for auxiliary functions in offroad applications, such as earthmoving and road equipment, but also for work functions on subcompact construction equipment where the available power is limited.Typical applications include signal light adjustment, ergonomic adjustment of seat height and position, safe opening and closing of heavy covers and engine hoods, roof height adjustment of open machines, swiveling of cabs and raising of jibs.
At bauma 2025, Schaeffler will also be showcasing its e-MOVEKIT, a preconfigured motor controller. The e-MOVEKIT is geared towards customers who want to procure all the necessary components to control an electromechanical actuator from a single source.
Efficient, durable and modular
The electromechanical linear actuator EMA-100 was designed to replace hydraulic cylinders on mini excavators and mini wheel loaders. The linear actuators feature a very compact design and broad range of mounting options.
The EMA-100 offers maximum drive forces of up to 60 kN in the version with ball screw and 82 kN in the case of a roller screw. Highly efficient, compact electric motors with holding brake are used as standard for the drive. With the help of an adapter, motors from all manufacturers can be installed if requested by the customer. The gear unit is flanged between the linear actuator and the motor and is available either as a spur gear or belt drive. However, the motor can also be mounted directly to the linear drive. Thanks to the high positioning accuracy and good controllability of the EMA-100 linear actuators via the bus system, several drives can be operated synchronously. Depending on the configuration, maximum linear speeds of up to 750 mm/s and stroke lengths of up to 2 m can be achieved.
					Publisher:  Schaeffler Technologies AG & Co. KG, Schweinfurt 
					Country: Germany
				
Terms of use for Schaeffler press pictures
Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.
We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.
Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.
Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany
Press releases
Package (Press release + media)