Schaeffler at bauma 2025 (Hall 6, Booth 103) Eco-friendly and durable: Maintenance-free plain bearings for kingpins and chassis joints in construction machinery
2025-04-03 | Schweinfurt
- New concept for replacing grease-lubricated rolling bearings with maintenance-free plain bearings with solid lubricant
 - Particularly eco-friendly bearing, as it does not require re-lubrication
 - Very positive test results in endurance tests
 
In construction machinery, rolling bearings are used, for example, as the bearing arrangement for kingpins and chassis joints. These bearing arrangements, which are subjected to high forces and strong shock loads, are characterized in particular by their swiveling movements at low speeds. Under these operating conditions, “false brinelling” – a wear phenomenon due to insufficient lubrication in the rolling contact – can occur on rolling bearings. Until now, the use of plain bearings has often foundered due to the high wear rate and excessively short re-lubrication intervals.
At bauma 2025 in Munich, Schaeffler will introduce a new concept to replace tapered rolling bearings on kingpins and chassis joints one for one with maintenance-free, dry-running plain (sleeve) bearings. These patented bearings are fitted with the high-performance Elgoglide sliding layer. Elgoglide withstands even high dynamic contact pressures of up to 300 N/mm2. Endurance tests with the new plain bearings under realistic conditions demonstrated extremely low rates of wear. The service lives required by construction machinery manufacturers are therefore readily achievable. The running-in wear that is customary with Elgoglide bearings, where solid lubricant particles are transferred from the sliding layer to the metal mating surface, is preempted by appropriate pre-loading of the bearing. Following the running-in phase, the bearings are backlash-free and run with a very low frictional torque.
Timo Linkert from Application Engineering at Schaeffler had this to say about the new plain bearings: “We see great potential for our Elgoglide bearings in kingpins and wheel suspensions because of the predominantly swiveling motions that Elgoglide bearings have proven capable of handling, even under high mechanical loads. The structure of the Elgoglide sliding layer also provides excellent shock absorption.” Moreover, these plain bearings from Schaeffler run dry, so there is no need for regular relubrication or considerable quantities of lubricating grease, which in turn protects the environment as there is no lubricating grease getting into the ground. The outer dimensions of the bearings being presented at bauma are the same as those of tapered rolling bearings, which substantially facilitates testing with series components and retrofitting of the current series. These bearing arrangements are generally developed to series maturity in close collaboration with Schaeffler’s engineers on a customer-specific basis.
					Publisher:  Schaeffler Technologies AG & Co. KG, Schweinfurt 
					Country: Germany
				
Terms of use for Schaeffler press pictures
Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.
We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.
Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.
Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany
Press releases
Package (Press release + media)