Search term

Schaeffler at bauma 2025 (Hall 6, Booth 103) Schaeffler presents innovative range of sensors for construction machinery

The torque measurement modules are based on the proven, non-contact sensor technology from Schaeffler. Image: Schaeffler
The torque measurement modules are based on the proven, non-contact sensor technology from Schaeffler. Image: Schaeffler

2025-04-03 | Schweinfurt

  • Sensorization for greater machine capacity utilization and availability
  • Schaeffler offers construction machinery manufacturers a range of customized sensors
  • Sensors detect overloads and critical operating conditions

Much like the industrial production segment, the construction sector also wants to use its machine pool to full capacity where possible and push construction machinery to its performance and loading limits while avoiding machine breakdowns. To achieve these objectives, the stress on machine components needs to be measured. The Motion Technology Company Schaeffler offers two solutions for achieving these ends: torque measurement modules and a unique sensorized metal pin.

Torque measurement module
The torque measurement modules are based on the proven, non-contact sensor technology from Schaeffler. Via an analog or CAN-bus interface, the data from the module captured during operation can be used e.g. for optimized control of operating functions, for safety functions, and for needs-based maintenance. Monitoring the torque allows the cumulative operating load to be evaluated, not just a recording of the operating hours of the respective drivetrain. The modules are generally developed as customized solutions. However, a deeper integration into the drivetrain is also possible. The magnetostrictive measuring principle offers exceptionally small hysteresis and high measuring accuracy.

Sensorized metal pin measures operating loads in components
The unique sensorized metal pin by Schaeffler allows stresses in metal components to be measured. It is pressed into a bore in the component and is therefore subject to the same stresses as the surrounding material. The pin has a strain-sensitive meander-shaped PVD (physical vapor deposition) coating on its surface that functions as a sensor element. With this small yet smart component, critical operating conditions and load peaks can be identified and operating costs reduced.

Sensors for clean combustion in diesel engines
At this year’s bauma, Schaeffler will also be showcasing components for exhaust gas aftertreatment in combustion engines. These will include NOx sensors with sensor control unit that have been incorporated into Schaeffler’s portfolio as a result of the merger with Tier 1 supplier Vitesco Technologies. Typically, two NOx sensors are used, one upstream and one downstream of the SCR catalytic converter (SCR = selective catalytic reduction). The NOx sensor upstream of the SCR catalytic converter measures the volume of nitrogen oxides being produced by the diesel engine. The engine control system uses these measured values to calculate the AdBlue dose for optimum reduction of the nitrogen oxides in the SCR catalytic converter. The NOx sensor downstream of the SCR catalytic converter monitors the functioning of the SCR catalytic converter. It measures how much NOx is still in the exhaust gas following the chemical reaction in the SCR system. Based on this data, the engine control system can adjust the AdBlue dose to ensure that the nitrogen oxide emission is minimized without consuming unnecessary amounts of urea solution. The sensor also recognizes whether the SCR catalytic converter is working properly or if there is a malfunction that could result in higher emissions. Thanks to the combination of the two sensors, a precise control of the exhaust gas aftertreatment is enabled, which helps to ensure compliance with the stringent statutory emission limits (Stage V) and optimize the consumption of fuel and AdBlue.

Publisher: Schaeffler Technologies AG & Co. KG, Schweinfurt
Country: Germany

Related media

Terms of use for Schaeffler press pictures

Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.

We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.

Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.

Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany

presse@schaeffler.com

Downloads

Package (Press release + media)

Share Page

Schaeffler applies cookies to secure an optimal use. With the further use of this website you accept the application of cookies. More Information

Accept