Schaeffler at bauma 2025 (Hall 6, Booth 103) On the road to decarbonization: Schaeffler presents e-motors with outputs of up to 315 kW
2025-04-03 | Schweinfurt
- Ready for volume production: the high-efficiency 800 V electric motor series for electric and hybrid drive systems
- Cost-effective production with automated coil manufacturing
- Especially high efficiencies for long operating times on construction sites
Today, there’s no longer any doubt that electric drive systems will make inroads into construction sites in the future. Some local governments in Germany and other countries are already banning vehicles with combustion engines from susceptible urban areas. At bauma 2025, Schaeffler will present its new high-performance heavy-duty electric motors as a volume production-ready solution for electric-only and hybrid drive systems. Due to their design, they achieve especially high torques, a power-to-weight ratio (peak) of around 5 to 7 kW/kg, and maximum efficiencies of more than 97% in a speed range of 3,000 to 8,000 rpm. The low losses of the liquid-cooled drive motors are essential to allow long operating times between charging cycles on construction sites and ensure efficient use of energy. Minimal losses and high operational reliability were also particularly important factors for the design of the bearing and seal. Ceramic balls reduce bearing friction and prevent damaging passage of current.
The modular motor series consists of three variants with maximum outputs of 125, 299 and 315 kW. The only difference is the length of the active parts. The individual stator laminations and the A- and B-side bearing end shields of the motors are identical in each case and therefore facilitate especially cost-efficient manufacturing. With an overall length of 151, 206 and 261 mm and a uniform outer diameter of around 239 mm (laminated core diameter) or 280 mm (including screw connection), the motors require minimal installation space. The stator windings are designed as flat wire (continuous hairpin) windings, also known as wave windings. At bauma in Munich, Schaeffler will be demonstrating a complete electric axle with integrated heavy-duty electric motor.
Schaeffler’s portfolio includes various types of electric motor and manufacturing technologies
Thanks to synergies from the automotive segment, the offroad sector of Schaeffler’s Bearings & Industrial Solutions division offers a comprehensive range of electric drives with a continuous output of 1 to 300 kW for the construction equipment industry. Schaeffler can supply a wide range of active-part components and complete systems such as wheel-hub drives based on permanent magnet synchronous machines. All crucial manufacturing technologies also come from a single source: the stator laminations stamped ‘in-house’, the hairpin and wave winding technology, the automatically produced coil windings, and the HV plug connector systems.
					Publisher:  Schaeffler Technologies AG & Co. KG, Schweinfurt 
					Country: Germany
				
Terms of use for Schaeffler press pictures
Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.
We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.
Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.
Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany
Press releases
Package (Press release + media)