Science Based Targets initiative (SBTi) validates Schaeffler's climate targets by 2035
2026-10-28 | Herzogenaurach
- SBTi validates the climate targets submitted by Schaeffler AG to reduce greenhouse gas emissions for 2035
- Absolute greenhouse gas emissions from Scope 1 and 2 are to be reduced by 42 percent by 2035 (base year: fiscal year 2025)
- Absolute Scope 3 emissions are to be reduced by 30 percent over the same period
- Schaeffler supports the Paris Agreement and aims to become a net-zero company by 2050
The Science Based Targets initiative (SBTi) has confirmed that the targets submitted by Schaeffler AG to reduce greenhouse gas emissions comply with the SBTi criteria and recommendations as so-called near-term targets.
Reducing absolute greenhouse gas emissions by 2035
The Schaeffler Group has further developed its sustainability strategy as part of the merger with Vitesco Technologies. Considering the significant reductions already achieved through the previous strategy during the pre-merger period, Schaeffler has now set itself the goal of reducing its absolute greenhouse gas emissions from Scope 1 and 2 by 42 percent by 2035 compared with the 2025 base year – which was the first fully consolidated year after the merger. The company has also set itself the goal of reducing absolute Scope 3 emissions from purchased goods and services, capital goods, fuel and energy activities, upstream transportation and distribution, waste in operations, and business travel by 30 percent over the same period.
Schaeffler CEO Klaus Rosenfeld says: "The validation of our climate targets by the Science Based Targets initiative marks an important milestone for Schaeffler on the path to climate neutrality. It means our climate targets are grounded in science, transparent and aligned with our responsibilities as a company. We recognize, however, that setting targets alone does not reduce emissions. The real work lies ahead. Further progress will be possible if we consistently align our actions with sustainability throughout our value chains. Following the acquisition of Vitesco, we are using 2025 as our new base year. We have a long-term perspective and are guided by our corporate values. For us, sustainability is both an obligation and an opportunity. Only by systematically integrating sustainability into our decisions and embedding it in our strategy can we lay the foundations for profitable growth and secure our long-term viability."
Support for the Paris Agreement
The Schaeffler Group supports the Paris Agreement and, in addition to the two climate targets validated by SBTi as so-called near-term targets, has set itself the goal – not validated by SBTi – of becoming a net-zero company by 2050. Schaeffler is committed to reducing Scope 1, 2, and 3 emissions by 90 percent by 2050 compared with the 2025 base year and to neutralizing remaining emissions in line with the applicable net-zero requirements. The framework for this is the "Climate Transition Plan", which was established in 2026 as part of the updated sustainability strategy.
Science-based and validated climate targets are targets that a company has submitted to the Science Based Targets initiative (SBTi) or SBTi Services. A formal review process confirms that these targets meet the SBTi's criteria in force at the time of submission.
The SBTi is a global organization that supports companies in setting science-based climate targets in line with the 1.5°C target of the Paris Climate Agreement. It develops standards, methods and guidelines for reducing greenhouse gas emissions and validates the climate targets submitted by companies.
The SBTi's validation information is available on the SBTi website.
Link to the Annual Report: Sustainability Statement, page 40:
Earnings releases | Schaeffler Group.
Publisher: Schaeffler AG
Country: Germany
Terms of use for Schaeffler press pictures
Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.
We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.
Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.
Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany
Press releases
Package (Press release + media)