Schaeffler at Agritechnica 2025 (Hall 15, Booth 15E13) Highly efficient electric motors for traction drives and auxiliary units in agriculture
2025-10-29 | Schweinfurt
- Modular 800 V electric motor series as traction drive and generator suitable for many types of vehicles and applications
- Cost-effective motor production with automated coil manufacturing
- Innovative wave winding technology ensures high power density
With an extensive product portfolio, the motion technology company Schaeffler is presenting itself at Agritechnica 2025 as a future-oriented systems supplier for agricultural machinery. Schaeffler’s heavy-duty electric motor platform was designed for a wide application spectrum of vehicles. Schaeffler’s electric motors can be used not only as fully electric traction drives, but also as generators in hybrid drives or even as a drive for an electric PTO. Schaeffler has end-to-end expertise in the production of technically demanding electric drives including controllers and power electronics.
Modular platform 
The 800 V heavy-duty platform consists of three oil-cooled motors, each developing 112 kW, 207 kW, and 220 kW continuous output. The only difference is the length of the active parts while the A- and B-sides of the motors are each identical. Schaeffler adopts the innovative ‘wave winding technology’ for the winding of the stator. This flat-wire wave winding makes for a very high copper filling ratio in the motor and results in a high-power density. This particular characteristic gives rise to a very compact motor that is optimized for continuous output. 
Through the integration of Vitesco Technologies as a provider of controllers and software, Schaeffler now has extensive, end-to-end expertise in the manufacture of technically complicated electric drives. All manufacturing technologies come from a single source.
Superlative efficiency in minimal space 
Due to their design, the heavy-duty electric motors achieve maximum efficiency of over 97 percent in a speed range from 3,000 to 8,000 rpm. With an overall length of 151, 206, and 261 mm with a uniform outside diameter of around 239 mm (laminated core diameter) or 280 mm (including screw connection), the motors take up minimal space. 
At Agritechnica in Hanover, Schaeffler will be demonstrating a complete electric axle with integrated heavy-duty electric motor.
					Publisher:  Schaeffler Technologies AG & Co. KG 
					Country: Germany
				
Terms of use for Schaeffler press pictures
Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.
We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.
Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.
Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany
Press releases
Package (Press release + media)