Schaeffler at bauma 2025 (Hall 6, Booth 103) Reducing the energy consumption of construction machinery with low-friction roller bearings
2025-04-03 | Schweinfurt
- Reduction of energy requirements and emissions of construction machinery by means of low-friction roller bearings in drivetrains and hydraulic pumps
 - Friction reduced thanks to optimized rib contact and surface structures
 - Energy-efficient optimization of bearing interior geometry for use in a wheel loader
 
By their very nature, rolling bearings are particularly low friction. However, in cylindrical and tapered roller bearings, there are sliding contacts that cause a high percentage of their frictional torque. Schaeffler’s development engineers have now been able to substantially reduce this proportion even more through targeted optimization measures.
Low-friction cylindrical roller bearings
There are various applications for cylindrical roller bearings in construction machinery. Accordingly, cylindrical roller bearings can be ideal for use in integrated planetary gear bearing arrangements. Here especially, they offer a major advantage in applications with minimal installation space and high radial load, and thanks to reduced friction can have a direct impact on the necessary energy consumption and thus the emissions of construction machinery.
Moreover, cylindrical roller bearings can substantially reduce the energy consumption of hydraulic pumps. Schaeffler engineers presented a use case where low-friction cylindrical and tapered roller bearings were used in the hydraulic system of a 140 kW wheel loader. The result in this case is that up to 9 kW can be saved by using X-life components and bearings with a hydraulic pump optimized in this way and two hydraulic motors. In the case of a fleet of 1,000 wheel loaders with normal operating times, 16,000 metric tons of CO2 can be saved a year.
Low-friction tapered roller bearings
Whereas conventional tapered roller bearings are already low friction, tapered roller bearings in X-life quality offer an additional increase in energy efficiency and load capacity. The rib contacts of the tapered roller bearings were optimized, while the surface structure, dimensional and running accuracy and material quality were substantially improved. The result is an increase in dynamic load ratings by up to 25 percent, which is associated with a doubling of service life. At the same, the frictional torque is reduced by up to 75 percent, compared with conventional products. These improvements also result in a significant reduction in the noise of the tapered roller bearings. In addition, targeted measures like an application-specific optimized internal geometry achieve reductions in friction that surpass the X-life quality.
					Publisher:  Schaeffler Technologies AG & Co. KG, Schweinfurt 
					Country: Germany
				
Terms of use for Schaeffler press pictures
Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.
We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.
Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.
Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany
Press releases
Package (Press release + media)