Schaeffler at Connecting Green Hydrogen Europe 2024, Booth H24 Schaeffler presents solutions for the industrial production of green hydrogen

2024-06-20 | Schweinfurt
- 1 MW PEM Electrolysis Stack as highlight
- Green hydrogen to support the energy transition
- Establishment of industrial series production in Herzogenaurach
Schaeffler will present its innovations for the production of green hydrogen at the Connecting Green Hydrogen Europe trade fair from June 25 to 27, 2024, in Madrid, Spain. The event will take place at IFEMA Madrid and will bring together experts and decision-makers from the hydrogen industry to discuss the latest trends and technologies. Schaeffler will showcase its new 1 MW Proton Exchange Membrane (PEM) electrolysis stack at its booth.
Schaeffler's PEM stacks, which feature a power rating of up to 1,000 kilowatts, are currently being introduced to the market. They can produce up to 500 kilograms of high-purity hydrogen per day.
"We provide key systems and components to make hydrogen technology future-proof. Our PEM electrolysis stacks are crucial sub-systems for a sustainable and efficient hydrogen production," says Florian Windisch, Head of Hydrogen at Schaeffler Bearings & Industrial Solutions.
Schaeffler is committed to a CO2-neutral, sustainable future and also recognizes the enormous potential of green hydrogen in this context. The Motion Technology Company considers the entire spectrum of applications – from the industrial production of green hydrogen via electrolysis to the use of hydrogen in fuel cells for both mobile and stationary applications, and even the production of green steel.
System integration for decentralized and centralized hydrogen production
The Schaeffler PEM electrolysis stacks are versatile and suitable for various industrial applications. By arranging the stacks in so-called arrays, Schaeffler can offer to the market flexible and powerful solutions ranging from 50 kW to multi-megawatt scales.
Industrialization expertise for scaling up the hydrogen economy
"Our long-standing industrialization expertise helps us turn innovations into efficient series production, thereby contributing to the creation of the conditions and capabilities necessary for scaling up hydrogen technology," says Florian Windisch. At Schaeffler's headquarters in Herzogenaurach, the industrial series production of stacks is currently being established.
With its core competencies in precise forming, joining and coating technology, and automated assembly technology by using processes and standards applicable for mass production, Schaeffler focuses on key pre-requisites for hydrogen technology.
Publisher: Schaeffler Technologies AG & Co. KG
Country: Germany
-
jpg | File size: 0.93 MBMW-class PEM (Proton Exchange Membrane) electrolysis stack in a test rig. Photo: Schaeffler
-
jpg | File size: 0.37 MBPEM electrolysis stack assembly line, Herzogenaurach, Germany. Photo: Schaeffler (Daniel Karmann)
Terms of use for Schaeffler press pictures
Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.
We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.
Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.
Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany
Press releases
Package (Press release + media)