Schaeffler at BrauBeviale in Hall 6, Booth 157 Schaeffler shows new approaches to lowering production costs in the beverage industry

2023-11-23 | Schweinfurt
- Portfolio ranges from standard rolling bearings to customized drive solutions
- Schaeffler’s OPTIME Ecosystem makes monitoring of machines and equipment particularly simple and economical
- Substantially reduced energy consumption: direct drive as alternative to geared motors
BrauBeviale, one of the leading capital goods fairs for the beverage industry worldwide, is due to take place in Nuremberg from November 28 to 30, 2023. Schaeffler will be on site with a presentation that focuses on solutions for economical and efficient beverage production.
Ralf Moseberg, Senior Vice President Industrial Automation at Schaeffler, points out: “The high cost pressures in the industry also have a positive side effect. Established series solutions are being questioned and the search for new and more efficient designs and solutions is beginning – and increasingly, this includes the entire life cycle of machines and systems. This is very much in line with our solutions for the food and beverage industry, from standard components and engineering to solutions for efficient operation and optimized maintenance.”
Safeguarding the brewing process with the OPTIME Ecosystem
The OPTIME Ecosystem not only provides brewers with an overview of the condition of all pumps and assemblies but also monitors lubricant supply. OPTIME Condition Monitoring (CM) is a system for the automatic monitoring of pumps, electric and geared motors, fans, rolling bearings and other assemblies of the kind often used in the beverage industry. The risk of unscheduled downtime is significantly reduced, which helps to achieve annual targets. Maintenance work can be planned and is more cost-efficient.
OPTIME C1, the first smart, automated lubricator on the market, is part of the OPTIME Ecosystem and uses the same technologies and user interfaces as OPTIME CM. Maintenance personnel are alerted via the Schaeffler OPTIME app about lubricators with a critical fill level, a fault in the lubrication supply and lubrication points with increased temperature.
Energy efficient beverage filling with direct drive systems
Worm gear motors are often used to drive star wheels in beverage filling machines. Although the drive power is just a few kilowatts, the annual losses add up to a considerable amount due to 24/7 operation and the low overall efficiency of 0.73-0.75. A direct drive like the Schaeffler RIB torque drive offers a significantly higher efficiency of 0.92 in this output class. Using this direct drive can save several tens of thousands of euros in energy costs and more than 100 tons of CO2 emissions over the life cycle of a single beverage filling line.
For the linear guides used in star wheels, Schaeffler recommends its KUVE-B series monorail guidance systems in combination with the KIT450 long-term lubricating units and a friction-optimized sealing assembly. The uniform distribution of the lubricant in the carriages reduces the amount of lubricant needed. By using these linear guides, operators can save around 50 percent lubricant and 70 percent maintenance costs. Service lives of more 50,000 km without relubrication are possible.
Automation and robotics: The beacons of hope in the beverage industry
At its exhibition booth, Schaeffler will use a Kuka IONTEC HO robot with barrel gripper to showcase its RT1 and RT2 series precision strain wave gears and configurable complete drives – known as drive systems – as well as the PSC range of precision planetary gear units. From the linear segment, 7th axes and new lifting columns will also be presented. For the automated transport and handling of bottles, boxes, drums and pallets, Schaeffler offers all bearing components, from simple linear bearings to portal handling and multi-axis systems.
Hygienic and easy to clean: Radial insert ball bearings in plastic housings
Radial insert ball bearing housing units are important components purchased by the beverage industry. Schaeffler offers a total of five housing variants in white plastic: two plummer block, two two-bolt and two four-bolt flanged units. The glass fiber reinforced PBT plastic is FDA-approved and is resistant to moisture, UV radiation, bacteriological and fungal attacks as well as many chemical media. All deep groove ball bearing components in the FD variant are in stainless steel. The allergen-free lubricating grease used in the bearings is approved to NSF category H1, meets the requirements of FDA21 CFR 178.3570, and is certified to halal and kosher standards.
Visit Schaeffler at the BrauBeviale trade show in Hall 6, Booth 157.
Publisher: Schaeffler Technologies AG & Co. KG
Country: Germany
Terms of use for Schaeffler press pictures
Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.
We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.
Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.
Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany
Press releases
Package (Press release + media)