Search term

Schaeffler Industrial at automatica 2023 in Hall B6, Booth 111 Focus on precision: Schaeffler showcases high-quality product range for robotics and Industrial automation

Pressrelease Stage Image
Premiere at automatica 2023: Precision drives for customized drive solutions Photo: Schaeffler

2023-06-26 | Schweinfurt

  • Schaeffler presents its complete range of precision strain wave gears and precision planetary gearboxes
  • Premiere: Modular and customized precision drives for industrial automation
  • Ewellix slide- and liftkits for robotics and automation solutions in various sectors

The Industrial division of the global automotive and industrial supplier Schaeffler is presenting its complete portfolio of precision bearings, precision gearboxes, and precision drives for industrial automation and specially for cobots and industrial robots at automatica 2023 (June 27 – 30, 2023 in Munich) in Hall B6, Booth 111.

Precision strain wave gears for cobots and lightweight robots
Schaeffler is presenting its compact precision strain wave gears of series RT1 (for the high-torque sector) and RT2 (for standard torque applications) as solutions for cobots and lightweight robots, but also for medical applications such as drives for C-arms and heavy ceiling mounts. RT1- and RT2-series precision strain wave gears are offered for output torques up to around 300 Nm. For output torques from 300 Nm to 5000 Nm, PSC-series precision planetary gearboxes are used.

The Ewellix slide- and liftkits are an ideal addition to the product range, which are used in preference as ready-to-fit horizontal and vertical axes to extend the range of cobots and industrial robots. Schaeffler is also presenting Ewellix floor lock actuators for the first time. These are very compact lifting units, which can be used to slightly raise mobile platforms such as autonomous mobile robots (AMR) or mobile tables or machine parts and thus firmly fix them to the floor.

Premiere at automatica: Individually configurable precision drives
The customer does have a large choice of suppliers in the market for precision servo drives, but usually only has a limited influence on their design. With the new precision drives from Schaeffler, companies can adapt the drives to largely match their application without having to invest in the development of these components. Essentially, the precision drives comprise the RT1- and RT2-series precision strain wave gears, which Schaeffler completes with selected motors, optional encoders, integrated torque sensor technology, and individually adapted housings and shafts to produce plug-&-play-ready drives. In this way, manufacturers can concentrate on their core expertise during the development of their machines, but do not have to do without customized drives.

In addition to Schaeffler’s Industrial division, Schaeffler Special Machinery – the Schaeffler Group’s Special Machinery sector – is also participating in the show again this year with a trade show booth in Hall A5, Booth 311.

Publisher: Schaeffler Technologies AG & Co. KG
Country: Germany

Related media

Terms of use for Schaeffler press pictures

Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.

We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.

Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.

Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany

presse@schaeffler.com

Downloads

Package (Press release + media)

Share Page

Schaeffler applies cookies to secure an optimal use. With the further use of this website you accept the application of cookies. More Information

Accept