Search term

Schaeffler at the MedtecLIVE in Hall 3C, Booth 415 Schaeffler shows components for increased safety and flexibility in medical technology

Pressrelease Stage Image
In the field of medical technology, Schaeffler offers a wide range of specialized rolling bearings and drive solutions for imaging, operating rooms, and laboratory automation, etc. (shown here as an example: C-arm application). Photo: Schaeffler

2023-05-22 | Schweinfurt

  • Schaeffler portfolio ranges from standard components through to customer-specific complete solutions
  • Rolling bearing and drive solutions for imaging processes, operating rooms, and laboratory automation
  • Lifting columns as well as the lifting and tilting module from the supplemented Ewellix range

The global automotive and industrial supplier Schaeffler is set to make its first appearance at the MedtecLIVE. This three-day trade show in Nuremberg will focus on the complete value-added chain of medical technology. Schaeffler is reflecting this in its portfolio, which ranges from standard components through to customer-specific complete solutions. Under the motto “Connecting the medical technology supply chain”, Schaeffler will present its new developments, which fulfill the high quality and safety requirements in the medical technology sector, offer increased reliability and flexibility, and extend the range of possible applications for medical equipment.

Ralf Moseberg, head of the Industrial Automation business unit at Schaeffler, emphasizes: “Medical technology is an established sector at Schaeffler. For computer tomography, for example, we have been offering customer-specific bearing and system solutions for more than two decades. These set the benchmark in terms of speeds, noise pollution, and frictional torque. Alongside robotics, medical technology is now one of our most important future markets. Both sectors are characterized by stable and strong growth as well as a high level of innovative strength.”

Rolling bearing solutions for imaging, hybrid operating rooms, and laboratory automation
Schaeffler is showing its wide range of specialized rolling bearings and drive solutions for imaging, operating rooms, and laboratory automation at its booth covering more than 100 square meters. One exhibit shows an X ray C-arm whose axes are completely equipped with bearings and linear guidance systems from Schaeffler. These include curved precision shafts with profiled track rollers in the C-arm. They are particularly smooth running, quiet, and, of course, can be set clearance-free. The fitted components also include slewing rings with mechanical and electromechanical brake, which are used in X ray C-arms and the ceiling mounts of operating rooms and intensive care wards.

In addition, Schaeffler is showing monorail guidance systems for horizontal movement of C arms and patient couches, such as those already used reliably in machine tool construction for many years.

An X ray bearing support in a vacuum from the Schaeffler Aerospace business unit, which can be used at temperatures of up to 500°C and speeds of up to 10,000 rpm, is also among the exhibits.

Schaeffler can now also cater for the last missing axis for C-arms – for height adjustment – as a result of the acquisition of Ewellix, which was completed at the beginning of 2023. Ewellix is one of the world’s leading manufacturers and suppliers of electromechanical actuators and lifting columns. “With the acquisition completed in January 2023, we have laid the foundation to become one of the world’s leading complete suppliers of linear technology and electromechanical actuator systems. Thanks to our expanded distribution network, a strong joint team, and a supplemented product portfolio, we are able to offer our customers worldwide very attractive solutions,” emphasizes Ralf Moseberg. The lifting and tilting module for operating table bearing supports also originates from the Ewellix range.

Precision gearboxes for the hybrid operating room
Schaeffler offers the PSC-series precision planetary gearbox and RT1 and RT2-series precision strain wave gears for both surgical robots and the movement of heavy ceiling mounts and ceiling mounted C-arms.

For laboratory automation, a new size of the UPLplus linear direct drive will be shown to complete the portfolio of linear guidance systems, drives, and multi-axis systems.

Visit Schaeffler at MedtecLIVE in Hall 3C, Booth 415.

Publisher: Schaeffler Technologies AG & Co. KG
Country: Germany

Related media

Terms of use for Schaeffler press pictures

Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.

We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.

Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.

Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany

presse@schaeffler.com

Downloads

Package (Press release + media)

Share Page

Schaeffler applies cookies to secure an optimal use. With the further use of this website you accept the application of cookies. More Information

Accept