Electric wheel hub motors go into production World premiere: Schaeffler electrifies municipal utility vehicles with in-wheel electric drives
![Pressrelease Stage Image](https://www.schaeffler.com/remotemedien/media/_shared_media_rwd/06_press/press_release/000015304_article_rwd_1000.jpg)
2023-03-23 | Bühl
- Schaeffler supplies first customers with fully electric wheel hub motors
- In-wheel electric drive makes road-sweeping vehicles, compact vans and snowplows quieter, more agile, and locally zero-emission
- New drive technology accelerates electrification of municipal utility vehicles and enables new vehicle architectures
With electrification, good things come in threes, it seems. No less than three manufacturers of compact municipal vehicles are gearing up to incorporate high-efficiency electric wheel hub motors made by Schaeffler into their production lines in the coming months. Fully electrified, their road sweepers, vans, and snowplow vehicles will operate with zero local CO2 emissions, leading to improved air quality in urban areas. “Schaeffler is reinventing the drive systems used in small, lightweight electric utility vehicles in our inner cities,” said Matthias Zink, Schaeffler’s CEO Automotive Technologies. The defining feature of the new wheel hub motors is that all the components needed for propulsion and braking are integrated directly into the wheel rim, rather than being positioned centrally or mounted on the drive axles. This architecture saves space and makes the vehicles much more agile and maneuverable in city traffic. Utility vehicles powered by these low-noise, fully electric motors are very quiet to operate, resulting in reduced sound pollution in pedestrian areas and on city streets. They can also be operated for extended hours in residential areas because the disturbance to residents is so much less.
One of the first companies to be launching a multifunction vehicle comprising Schaeffler wheel hub motor technology onto the market this year is Jungo. Jungo and Schaeffler have been partnering to tailor the drive technology to the specific everyday requirements of commercial street sweeping. “The electric in-wheel motors and braking technology eliminates the need for oil changes and greatly enhances our vehicles’ performance in terms of efficiency, power-to-weight ratio, safety, handling, and braking reliability,” said Jungo founder and CEO Nicolas Jungo.
Efficient solution for a wide range of inner-city and mobility scenarios
Schaeffler’s wheel hub motors have a broad range of inner-city mobile machinery applications, including street sweeping, snow clearing, and waste collection. “In this vehicle segment, as in others, the question is: what’s the fastest and most efficient way to reduce CO2 emissions? And the answer to that question is electrification,” said Dr. Jochen Schröder, head of E-Mobility at Schaeffler. This new drive technology opens up a new and steadily growing market for Schaeffler. The company aims to see its wheel hub motors used in more and more utility and service vehicles in towns and cities, on factory campuses, and at logistics centers, ports, airports, and large parking facilities. These types of vehicles tend to be operated on set routes, so they are a good fit for the fixed ranges and predictable charging times of electric drives. Another key benefit for vehicle operators is that the wheel hub motors have long-life, low-maintenance wheel bearings and gearboxes.
Schaeffler’s fully electric wheel hub motors have a unique architecture in which the electric motor (stator and rotor), gearbox, and mechanical friction brake are arranged around the wheel bearing inside the rim. This compact design envelope frees up space elsewhere in the vehicle – for the battery or cargo stowage, for example. It also gives vehicle manufacturers greater design freedom, allowing them to develop a wide range of mobility formats, including rolling chassis solutions. “Our highly integrated electric wheel hub motors also improve vehicle maneuverability, which is a key prerequisite for automated driving,” said Jochen Schröder.
In-wheel motor saves space and improves driving dynamics
The wheel hub motor, including the gearbox, is very compact, fitting inside a 14-inch rim. The inverter, on the other hand, is not integrated, and can be accommodated anywhere in the vehicle. A single inverter controls one or two wheel hub motors, depending on the use scenario. The motor’s power output is scalable, depending on the application, ranging from 7 kW to 26 kW (nominal) and peaking at 60 kW for short bursts. The torque generated by the electric motor is transmitted via the gearbox directly to the wheel. This direct transmission reduces energy loss, making the drive highly efficient. Another key benefit is that torque and direction of rotation are controlled individually for each wheel, resulting in an all-wheel drive vehicle that can handle hills with consummate ease, even in winter road conditions. Schaeffler currently develops wheel hub motors for 48 V and 400 V applications and is exploring the possibility of higher voltages.
Further information
Technical article on wheel hub motors and rolling chassis solutions by Schaeffler
Publisher: Schaeffler Automotive Bühl
Country: Germany
Terms of use for Schaeffler press pictures
Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.
We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.
Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.