Schaeffler at Hannover Messe 2022, hall 6, booth C48 Schaeffler Lubtect for Safe Use in the Food Industry
2022-04-06 | Schweinfurt
- Schaeffler expands its range of bearing solutions for the food industry
- Lubricant compound Lubtect is available for deep groove ball bearings, tapered roller bearings, spherical roller bearings, cylindrical roller bearings, and needle roller bearings
- Lubricant compound Lubtect available with NSF H1 approval
The lubricant compound Schaeffler Lubtect offers an option for keeping lubricant even safer inside the bearing. Especially in food processing, the prevention of contamination plays an important role. This compound fills the cavity in rolling bearings, which are sealed on both sides. The lubricant is permanently stored in the porous structure of the compound, thus minimizing, if not eliminating, the risk of contamination from escaping lubricant. The bearings are lubricated for life. Relubrication, and hence the potential unprotected use of grease guns in these particularly sensitive application areas, is also no longer required. This contributes to the overall safety of the facility, which is particularly important for the food and animal feed industries. Even at low ambient temperatures, good lubricant distribution is ensured, thus enabling a longer bearing operating life. Lubtect is available for deep groove ball bearings, tapered roller bearings, spherical roller bearings, cylindrical roller bearings, and needle roller bearings. Schaeffler received H1 approval from the US organization NSF International authorizing the use of Lubtect in sensitive application areas. Lubtect is also halal and kosher certified.
Publisher: Schaeffler AG
Country: Germany
Terms of use for Schaeffler press pictures
Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.
We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.
Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.