Schaeffler at InnoTrans 2024 (Hall 21, Booth 430) Smart Maintenance Tools for safe and efficient maintenance
2024-09-18 | Schweinfurt
- Expanded range of tools under the “Smart Maintenance Tools” label
- Self-centering mechanical and hydraulic extractors for fast, easy handling
- Thermal tools for fast, material-friendly, energy-saving mounting operations
Between 10 and 20 percent of all bearing failures are caused by incorrect handling during maintenance. Accordingly, at InnoTrans 2024, Schaeffler is showcasing its Smart Maintenance Tools (formerly Bega Special Tools), an expanded range of solutions for the ergonomic, safe and material-friendly mounting and dismounting of powertrain components.
Hydraulic and mechanical extractors
The Schaeffler display includes self-centering mechanical and hydraulic 2- and 3-arm extractor tools from its MSP (mechanical), HSP and HXP (hydraulic) series of products for the safe, easy mounting of small to medium-size components.
In terms of handling solutions specifically for large rail and metro bearings, couplings and wheels, Schaeffler is presenting the BETEX HXPM, which has a maximum pulling capacity of 150 tons, and the BETEX BPP, which has a maximum capacity of 100 tons. These tools are height-adjustable and easy to maneuver, so they can be operated quickly, easily and safely – even by a single technician working on their own. Moreover, the intelligent tool design minimizes the risk of damage to axles and to the bearings and wheels being mounted or dismounted. Both types of tool – mechanical and hydraulic – are self-centering. 
Thermal bearing tools
For mounting and dismounting large workpieces, Schaeffler also offers mobile and highly versatile induction heaters featuring Medium-Frequency Technology (MFT). Thanks to their shorter heating times, these heaters cut bearing mounting and dismounting times in half. This productivity gain dramatically reduces maintenance costs. 
Schaeffler’s “HEATER”-series induction heating devices are used for fast and gentle heating of complete rolling bearings, inner rings of rolling bearings and other rotary machine elements that have to be fixed onto a shaft and thermally expanded before assembly.
					Publisher:  Schaeffler Technologies AG & Co. KG, Schweinfurt 
					Country: Germany
				
Terms of use for Schaeffler press pictures
Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.
We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.
Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.
Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany
Press releases
Package (Press release + media)