Schaeffler at InnoTrans 2024 (Hall 21, Booth 430) Efficiency and reliability: TAROL axlebox bearings for passenger, freight and heavy goods transport
2024-09-18 | Schweinfurt
- Now certified according to AAR standard as well as EN 12080
- Application-optimized products through customer-specific design
- Friction-optimized seals for a wide range of applications
Low-friction TAROL axlebox bearings facilitate more reliable and economical rail operations and are one of Schaeffler’s main exhibits at InnoTrans 2024. The showcase includes TAROL axlebox bearings developed for the AAR (Association of American Railroads) market. These bearings meet the certification requirements under both the AAR and European standards, so they can be used in the USA, Australia, India, Southeast Asia and many other countries and regions in addition to Europe. Characterized by long service life and significantly extended maintenance intervals, they ensure reliable operation.
The superior reliability of Schaeffler’s double-row tapered roller bearings is the result of the company’s comprehensive systems know-how. In the case of the TAROL axlebox bearings, this superior know-how finds expression in a well-integrated unit comprising rolling bearings, seals, lubricant and a housing. The result is above-average reliability and robustness even under extreme loads. Thanks to customer-specific design, the bearing dimensions and materials can be optimally matched to the required payload and mileage. Schaeffler offers a range of variants for different applications. For example, the TAROL GG variant is specifically designed for freight transport locomotives, while the high-capacity Class K variant is optimized for heavy goods transport. Both bearings are supplied with friction-optimized seals and thus make an important contribution to reducing CO₂ emissions in rail transport operations.
					Publisher:  Schaeffler Technologies AG & Co. KG, Schweinfurt 
					Country: Germany
				
Terms of use for Schaeffler press pictures
Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.
We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.
Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.
Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany
Press releases
Package (Press release + media)