Schaeffler at InnoTrans 2024 (Hall 21, Booth 430) Equal to extreme loads: Current-insulated bearings and hybrid cylindrical roller bearings
2024-09-18 | Schweinfurt
- Reliable traction motor bearings for improved cost-effectiveness
- Electrically insulated traction motor bearings prevent damage and save on costly repairs
- High-capacity cylindrical roller bearings with single-piece solid-brass cage available as standard
How can rail vehicles be made even more reliable and cost-effective to operate? Schaeffler has developed an answer to this question – in the form of exceptionally reliable traction motor bearings that prevent damage and avoid costly repairs and downtime.
A key way to improve reliability is to use current-insulated rolling bearings featuring the Insutect A ceramic coating. In rail vehicles, the operation of electric motors can cause unwanted electric currents in wheelsets, gearboxes and traction motors. This can damage raceways and rolling elements and cause lubricants to break down, resulting ultimately in premature and unexpected component failures. All of which translates into higher maintenance and repair costs, not to mention the added expense of machine downtime. Schaeffler offers a cost-effective and reliable solution to this problem with its electrically insulated bearings. These ceramic-coated bearings and hybrid bearings with ceramic rolling elements reduce maintenance costs and increase machine availability.
New solutions are needed to meet constantly growing demands and loads on machine components. That’s why the Schaeffler innovations on show at InnoTrans also include high-capacity cylindrical roller bearings for traction-motors, featuring the new single-part “MP” solid brass cage. Compared with the “M1” two-piece, riveted solid brass cage, this new cage offers higher strength under stresses caused by vibrations and shocks, even at higher rotational speeds. The new cage design also simplifies bearing reconditioning because the rollers can be removed without damaging the cage. The benefits to customers include optimized operational reliability, longer service life, and reduced lifecycle costs and total cost of ownership (TCO). The longer service life also improves rail operators’ carbon footprint.
					Publisher:  Schaeffler Technologies AG & Co. KG, Schweinfurt 
					Country: Germany
				
Terms of use for Schaeffler press pictures
Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.
We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.
Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.
Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany
Press releases
Package (Press release + media)