Suchbegriff

Schaeffler at Maintenance Dortmund 2026 Innovative solutions for efficient lubrication, smart condition monitoring, and safe mounting

At Maintenance Dortmund, Schaeffler will demonstrate the mounting and dismounting of bearings live at the booth with the help of the MF Generator 3.0.
At Maintenance Dortmund, Schaeffler will demonstrate the mounting and dismounting of bearings live at the booth with the help of the MF Generator 3.0. The generator is based on an induction system using medium-frequency technology, offers an output of 3.5 kW, and is ideal for mounting and dismounting of small to medium-sized workpieces. (Image: Schaeffler)

12.02.2026 | Schweinfurt

  • Medium-frequency induction ensures fast and safe mounting and dismounting of bearings
  • Arcanol lubricants extend the service life of bearings and linear motion systems
  • FAG OPTIME E-CM monitors electric motors and reduces downtime

The Motion Technology Company Schaeffler will be at the Maintenance Dortmund trade show to present innovative technologies and solutions that take customers’ industrial maintenance processes, manufacturing efficiency, and plant availability to whole new levels.

Focus will be on three main thematic areas: state-of-the-art medium-frequency induction systems for enabling fast, safe mounting and dismounting of bearing components, the proven Arcanol lubricants for extending the service life of rolling bearings, and the OPTIME Ecosystem for smart condition monitoring.

Medium-frequency induction systems: Efficient mounting and dismounting
With the medium-frequency induction systems, Schaeffler offers a fast, safe, and energy-efficient solution for the controlled heating of bearings and other components. Unlike low-frequency heaters, the medium-frequency systems can be used not just for mounting but also for dismounting.

The inductive heating and the precise expansion of parts ensure easy mounting and dismounting. The generators are available in 3.5 kW to 44 kW variants and can be used with a vast array of differently sized and shaped workpieces, ranging from small bearing rings to large components such as main bearings or the housings of wind turbines.

At Maintenance Dortmund, Schaeffler will also be demonstrating the mobile MF Generator 3.0 live at the booth. With 3.5 kW, this generator is ideal for small to medium-sized workpieces and flexible on-site use.

Extended service life with the right lubricant
An often underestimated but decisive factor determining the service life of rolling bearings is the lubricant used. Arcanol lubricants from Schaeffler stand out due to their ability to significantly reduce friction and wear in rotary and linear bearings. This in turn results in a longer service life and greater sustainability. The product portfolio offers a wide range of specially developed lubricants that are tailored to different operating conditions such as temperatures, loads, and environments. The consistently high quality and reliability of each batch is ensured through rigorous physical and chemical testing. Visitors to the Schaeffler booth can find out about the innovative testing methods used as well as the performance capabilities and the wide range of applications of the Arcanol lubricants.

FAG OPTIME E-CM: Electrical condition monitoring of three-phase motors
The Schaeffler OPTIME Ecosystem is a leading solution for smart machine monitoring and intelligent lubrication. The portfolio has recently been supplemented by the FAG OPTIME E-CM system for the electrical condition monitoring of three-phase motors – one of the main types of drives used in compressors, rotary pumps, fans, and grinding machines. Whereas the predecessor OPTIME sensors primarily offered early detection of mechanical vibrations, the FAG OPTIME E-CM supplements this with analysis of motor currents and voltages. This combination makes it possible to predict failures even more reliably and prevent unplanned downtimes even more effectively than before.

Herausgeber: Schaeffler Technologies AG & Co. KG
Ausgabeland: Deutschland

Zugehörige Medien

Nutzungsbedingungen für Schaeffler-Pressebilder

Schaeffler-Pressebilder dürfen ausschließlich für redaktionelle Zwecke verwendet werden. Sofern nichts anderes angegeben, liegen sämtliche Urheber-, Nutzungs- und Verwertungsrechte bei der Schaeffler Technologies AG & Co. KG, Herzogenaurach, oder bei einem ihrer verbundenen Unternehmen. Die Vervielfältigung und die Veröffentlichung der Schaeffler-Pressebilder ist nur mit Angabe der Quelle wie folgt „Bild: Schaeffler“ gestattet. In diesem Fall ist die Verwendung honorarfrei möglich. Die Befugnis zur Verwendung zu werblichen oder sonstigen kommerziellen Zwecken, insbesondere zur kommerziellen Weitergabe an Dritte, wird hiermit nicht eingeräumt. Bearbeitungen bedürfen in jedem Fall der Zustimmung von Schaeffler.

Bei Veröffentlichung von Schaeffler-Pressebildern in Printmedien bitten wir um die Zusendung eines Belegexemplars (bei Veröffentlichung in elektronischen Medien um ein digitales Exemplar bzw. einen Link). Bei Verwendung von Schaeffler-Pressebildern in Filmen bitten wir um Benachrichtigung und Angabe des Filmtitels.

Die Nutzung der Schaeffler-Pressebilder unterliegt deutschem Recht mit Ausnahme des Kollisionsrechts, Gerichtsstand ist Nürnberg, Deutschland.

Adresse:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestraße 1-3
91074 Herzogenaurach
Deutschland

presse@schaeffler.com

Downloads

Pressemitteilungen

Paket (Pressemitteilung + Medien)

Seite teilen

Schaeffler verwendet Cookies, um Ihnen eine optimale Nutzung zu gewährleisten. Durch die weitere Nutzung dieser Website stimmen Sie der Verwendung von Cookies zu. Weitere Informationen

Akzeptieren