Schaeffler and Humanoid enter strategic technology partnership
13.01.2026 | Herzogenaurach, Germany/London, UK
- Schaeffler and British technology company Humanoid form strategic partnership to develop innovative components for humanoid robots
- Partnership includes supply agreement for actuators and purchase agreement for humanoids for Schaeffler’s global production network
- Another milestone for Schaeffler in its quest to become a preferred technology partner in the humanoid robotics segment
Schaeffler continues to strengthen its position as a preferred technology partner for humanoid robotics by establishing a strategic technology partnership with British technology company Humanoid. The collaboration will focus on the development and supply of key components, including innovative actuators used in both wheeled-base and bipedal (two-legged) humanoids. Schaeffler is becoming the preferred supplier of actuators for wheeled systems. Moreover, Schaeffler is planning to integrate several hundred humanoids into its global production network over the next five years to further increase the automation and efficiency of its production processes. Together, both companies are collecting robot-specific and application-related data, to train AI models and continually optimize robot performance.
Klaus Rosenfeld, CEO of Schaeffler AG, says: “As a Motion Technology Company, we want to play a key role in the growing humanoid robotics market. To do so, we are relying on our decades-long manufacturing excellence and industrialization expertise. With Humanoid, we are gaining an attractive partner in Europe that will enable us to drive forward joint innovations in the field of humanoid robotics.”
Artem Sokolov, CEO and founder of Humanoid, says: “For years, humanoid robotics has been taking place in labs, product demonstrations and ‘proof-of-concepts’, but real-life application in large volumes is the moment when the technology will truly be put to the test. At Humanoid, we firmly believe that the future of humanoid robotics will not be defined by the most impressive demonstrations but by its large-scale scalability and capacity for use in real-world environments. This large-scale use is an important step towards this future. It allows us to validate humanoids under real-world conditions and create a clear pathway to commercial use in the next few years. Together with Schaeffler, we will prove that humanoids can work in industrial environments reliably, safely and efficiently.”
Actuator expertise for precise humanoid movements
Schaeffler offers an extensive range of products for humanoids, including scalable solutions like linear and rotary actuators for precise movements in robot joints. A key component of the partnership with Humanoid is the development and supply of Schaeffler strain wave gear actuators. These are produced using innovative manufacturing processes, including winding, surface mounting, and machining technology as well as assembly and testing technologies that ensure outstanding quality and reliability. Strain wave gear actuators are used primarily in the upper body, shoulders and arms of humanoid robots. Thanks to their outstanding weight/torque ratio and a large hollow shaft, they enable complete internal cabling of the actuators and extremities. The design is optimized for large production volumes and offers zero backlash, low friction, and excellent precision – ideal conditions for dynamic use and continuous load capacity in modern humanoid robots.
Andreas Schick, Chief Operating Officer of Schaeffler AG and the Executive Board member responsible for the company’s humanoid activities, says: “Humanoid robots represent movement and precision at their best. With our comprehensive manufacturing excellence in high volumes, and strong vertical integration, we offer innovative products in the highest quality. The close integration of our development and production allows us to realize customized solutions that will take modern humanoid robots to a new level.”
Forward-looking statements and projections
Certain statements in this press release are forward-looking statements. By their nature, forward-looking statements involve a number of risks, uncertainties and assumptions that could cause actual results or events to differ materially from those expressed or implied by the forward-looking statements. These risks, uncertainties and assumptions could adversely affect the outcome and financial consequences of the plans and events described herein. No one undertakes any obligation to publicly update or revise any forward-looking statement, whether as a result of new information, future events or otherwise. You should not place any undue reliance on forward-looking statements which speak only as of the date of this press release. Statements contained in this press release regarding past trends or events should not be taken as representation that such trends or events will continue in the future. The cautionary statements set out above should be considered in connection with any subsequent written or oral forward-looking statements that Schaeffler, or persons acting on its behalf, may issue.
Herausgeber: Schaeffler AG
Ausgabeland: Deutschland
Nutzungsbedingungen für Schaeffler-Pressebilder
Schaeffler-Pressebilder dürfen ausschließlich für redaktionelle Zwecke verwendet werden. Sofern nichts anderes angegeben, liegen sämtliche Urheber-, Nutzungs- und Verwertungsrechte bei der Schaeffler Technologies AG & Co. KG, Herzogenaurach, oder bei einem ihrer verbundenen Unternehmen. Die Vervielfältigung und die Veröffentlichung der Schaeffler-Pressebilder ist nur mit Angabe der Quelle wie folgt „Bild: Schaeffler“ gestattet. In diesem Fall ist die Verwendung honorarfrei möglich. Die Befugnis zur Verwendung zu werblichen oder sonstigen kommerziellen Zwecken, insbesondere zur kommerziellen Weitergabe an Dritte, wird hiermit nicht eingeräumt. Bearbeitungen bedürfen in jedem Fall der Zustimmung von Schaeffler.
Bei Veröffentlichung von Schaeffler-Pressebildern in Printmedien bitten wir um die Zusendung eines Belegexemplars (bei Veröffentlichung in elektronischen Medien um ein digitales Exemplar bzw. einen Link). Bei Verwendung von Schaeffler-Pressebildern in Filmen bitten wir um Benachrichtigung und Angabe des Filmtitels.
Die Nutzung der Schaeffler-Pressebilder unterliegt deutschem Recht mit Ausnahme des Kollisionsrechts, Gerichtsstand ist Nürnberg, Deutschland.
Adresse:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestraße 1-3
91074 Herzogenaurach
Deutschland
Pressemitteilungen
Paket (Pressemitteilung + Medien)