Schaeffler and Sonatus bring Edge AI to motion control for software-defined vehicles
10.06.2026 | Herzogenaurach, Germany - Sunnyvale (CA), USA
- Schaeffler and Sonatus incorporate Edge AI into motion control to accelerate the shift to centralized electrical and electronic architectures
- Sonatus software is seamlessly integrated into Schaeffler control units, reducing integration and validation effort for OEMs
- The partnership strengthens Schaeffler’s position as a system and software partner for software-defined vehicles
Schaeffler and Sonatus, a leader in intelligence-driven, software-defined vehicle technology, announced a global partnership to bring Edge AI into motion control solution for software-defined vehicles (SDVs).
By combining Schaeffler’s control units with Sonatus’ AI-infrastructure software, the companies enable intelligence directly at the vehicle edge – accelerating development, reducing complexity, and unlocking continuous improvement throughout the vehicle lifecycle.
Software-defined vehicles require more than powerful hardware – they depend on seamless interaction between hardware, software, and data. The joint solution integrates Sonatus Collector AI and Sonatus AI Director into Schaeffler’s control units, creating a ready-to-use foundation for next-generation vehicle architectures, and ensuring a faster time to market.
“Software-defined vehicles require a robust and scalable hardware foundation,” says Thomas Stierle, CEO E-Mobility at Schaeffler AG. “Our control units run data-driven and AI-based functions within the vehicle, enabling the next generation of vehicle architectures.”
From hardware to intelligent systems
As Motion Technology Company, Schaeffler contributes its cross-domain control units and comprehensive system integration expertise across powertrain, energy, chassis, and body domains – enabling centralized and zonal architectures that form the backbone of an SDV.
Sonatus brings to the partnership a proven track record in production-grade, AI-driven technology for software-defined vehicles that is deployed in more than 8 million vehicles. Its solutions extend Schaeffler’s systems with embedded AI capabilities:
- Sonatus Collector AI enables targeted, real-time data collection without relying on large-scale data logging
- Sonatus AI Director allows the deployment and lifecycle management of AI models directly on the vehicle
"Hardware centralization is the first step; the software-defined vehicle is realized when AI can be running at the edge and when hardware continuously learns and adapts. Together with Schaeffler, we are turning static control units into dynamic, intelligence-driven systems,” says Jeff Chou, CEO and Co-Founder of Sonatus.
Clear benefits for OEMs
The solution developed by the partners allows automakers to run and continuously improve key vehicle functions – such as steering, braking, and energy management – directly on the control unit. New features and optimizations can be deployed over the vehicle’s lifecycle without hardware changes.
Flexible data collection enables faster issue resolution and deeper insights into vehicle performance, equipping OEMs to better manage increasing system complexity while significantly accelerating development cycles.
The partnership underlines Schaeffler’s strategic focus on software and systems engineering for software-defined vehicles. By combining hardware, embedded software and system integration expertise, Schaeffler helps its customers to manage increasing system complexity and accelerate the adoption of future vehicle architectures.
“Our central control units are equipped with a pre-integrated software infrastructure that includes solutions such as Sonatus products. This significantly simplifies integration for our customers and helps them accelerate the centralization of their software architecture,” says Rodrigo Peres, Senior Vice President of Business Unit Vehicle and Battery Controls at Schaeffler AG.
About Sonatus
Sonatus is a leading technology provider for intelligence-driven software-defined vehicles that are scalable and upgradable. Our AI solutions and software-defined technologies empower OEMs and suppliers to reduce costs, accelerate time-to-market, and deliver uncompromised quality. Founded in 2018, Sonatus is privately held, backed by leading investors spanning the automotive, semiconductor, and venture capital sectors, and its technology is in more than 8 million production vehicles from leading global automakers. Sonatus is headquartered in Sunnyvale, Calif. (Silicon Valley), with regional headquarters in Dublin, and offices in Bangalore, Detroit, Frankfurt, Kraków, Paris, Pune, Seoul, Shanghai, Taipei, and Tokyo. For more information, visit www.sonatus.com.
Herausgeber: Schaeffler AG
Ausgabeland: Deutschland
Nutzungsbedingungen für Schaeffler-Pressebilder
Schaeffler-Pressebilder dürfen ausschließlich für redaktionelle Zwecke verwendet werden. Sofern nichts anderes angegeben, liegen sämtliche Urheber-, Nutzungs- und Verwertungsrechte bei der Schaeffler Technologies AG & Co. KG, Herzogenaurach, oder bei einem ihrer verbundenen Unternehmen. Die Vervielfältigung und die Veröffentlichung der Schaeffler-Pressebilder ist nur mit Angabe der Quelle wie folgt „Bild: Schaeffler“ gestattet. In diesem Fall ist die Verwendung honorarfrei möglich. Die Befugnis zur Verwendung zu werblichen oder sonstigen kommerziellen Zwecken, insbesondere zur kommerziellen Weitergabe an Dritte, wird hiermit nicht eingeräumt. Bearbeitungen bedürfen in jedem Fall der Zustimmung von Schaeffler.
Bei Veröffentlichung von Schaeffler-Pressebildern in Printmedien bitten wir um die Zusendung eines Belegexemplars (bei Veröffentlichung in elektronischen Medien um ein digitales Exemplar bzw. einen Link). Bei Verwendung von Schaeffler-Pressebildern in Filmen bitten wir um Benachrichtigung und Angabe des Filmtitels.
Die Nutzung der Schaeffler-Pressebilder unterliegt deutschem Recht mit Ausnahme des Kollisionsrechts, Gerichtsstand ist Nürnberg, Deutschland.
Adresse:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestraße 1-3
91074 Herzogenaurach
Deutschland
Pressemitteilungen
Paket (Pressemitteilung + Medien)