CES 2026 Schaeffler presents innovative planetary gear actuator for humanoid robots
16.12.2025 | Las Vegas/ Herzogenaurach
- Schaeffler’s planetary gear actuator ensures precise movements in robot joints and enables continuous-duty operation
- Innovative actuator system combines a two-stage planetary gearbox, electric motor, encoder, and controller in a compact unit
- Decades of Schaeffler actuator expertise make humanoid robots even more capable and powerful
World premiere at the Consumer Electronics Show 2026 (CES) in Las Vegas: For the first time, Schaeffler is presenting a planetary gear actuator developed specifically for humanoid robots at a leading global trade fair. Actuators transmit torque with high precision and minimal compliance and are essential for enabling humanoid robots to move accurately and efficiently. On average, 25 to 30 actuators are required in total for joints such as the shoulders, knees, and hips. While conventional actuators often offer limited or no back-drive-ability – that is, the ability to move the drive in reverse – Schaeffler’s planetary gear actuator enables smooth back-driving and high precision thanks to its innovative design. In addition, Schaeffler manufactures all components entirely in-house, ensuring the highest levels of quality and reliability. Humanoid robots will play a key role in the industry of tomorrow, as they can be seamlessly integrated into existing work environments, relieve employees of repetitive and ergonomically demanding tasks, and significantly increase productivity as a result.
Andreas Schick, Chief Operating Officer of Schaeffler AG and responsible on the Executive Board for humanoid activities, says: “Schaeffler aims to secure a key position in the rapidly growing humanoid robotics market. Thanks to our decades of manufacturing expertise, we are able to deliver the highest quality in large volumes and within the shortest possible production times. The innovative planetary gear actuator is a production-ready key product within our portfolio and will make humanoid robots even more capable and powerful.”
Planetary gear actuator: A tailor-made drive solution for humanoid robots
Schaeffler deploys humanoid robots across its entire value chain and therefore understands market requirements and customer needs firsthand. This enables Schaeffler to successfully transfer scalable solutions from the automotive and industrial sectors to humanoid robotics and to develop tailor-made products that address the challenges of the future. With a comprehensive portfolio spanning eight product families, Schaeffler covers the full spectrum of requirements for humanoid robots. Integrated linear and rotary actuators – one of Schaeffler’s core competencies – account for around half of all components in a humanoid robot. This highlights the company’s strong vertical integration and its concentrated expertise as a Motion Technology Company.
One of the product highlights of this year’s CES trade show is the planetary gear actuator, a highly efficient drive system designed and manufactured entirely by Schaeffler. The compact yet powerful system combines a two-stage planetary gearbox, an electric motor, as well as an encoder and controller in a space-optimized unit. Thanks to its high thermal stability, a torque range of 60 to 250 Nm, and particularly low back-drive-ability, the planetary gear actuator withstands external forces and prevents unintended reverse rotation of the drive component. The result is precise, energy-efficient motion sequences with high torque transparency – ideal for continuous-duty operation in humanoid robots.
Schaeffler at the Consumer Electronics Show
Innovative key components for humanoid robots, along with other future technologies from Schaeffler, will be on display from January 6 to 9, 2026, in the West Hall of the Las Vegas Convention Center at Booth 7301.
Learn more about Schaeffler’s appearance at the Consumer Electronics Show:
CES 2026 | Dates & Events | Schaeffler Group USA Inc.
Herausgeber: Schaeffler AG
Ausgabeland: Deutschland
Nutzungsbedingungen für Schaeffler-Pressebilder
Schaeffler-Pressebilder dürfen ausschließlich für redaktionelle Zwecke verwendet werden. Sofern nichts anderes angegeben, liegen sämtliche Urheber-, Nutzungs- und Verwertungsrechte bei der Schaeffler Technologies AG & Co. KG, Herzogenaurach, oder bei einem ihrer verbundenen Unternehmen. Die Vervielfältigung und die Veröffentlichung der Schaeffler-Pressebilder ist nur mit Angabe der Quelle wie folgt „Bild: Schaeffler“ gestattet. In diesem Fall ist die Verwendung honorarfrei möglich. Die Befugnis zur Verwendung zu werblichen oder sonstigen kommerziellen Zwecken, insbesondere zur kommerziellen Weitergabe an Dritte, wird hiermit nicht eingeräumt. Bearbeitungen bedürfen in jedem Fall der Zustimmung von Schaeffler.
Bei Veröffentlichung von Schaeffler-Pressebildern in Printmedien bitten wir um die Zusendung eines Belegexemplars (bei Veröffentlichung in elektronischen Medien um ein digitales Exemplar bzw. einen Link). Bei Verwendung von Schaeffler-Pressebildern in Filmen bitten wir um Benachrichtigung und Angabe des Filmtitels.
Die Nutzung der Schaeffler-Pressebilder unterliegt deutschem Recht mit Ausnahme des Kollisionsrechts, Gerichtsstand ist Nürnberg, Deutschland.
Adresse:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestraße 1-3
91074 Herzogenaurach
Deutschland
Pressemitteilungen
Paket (Pressemitteilung + Medien)