Schaeffler SmartUtility Release Notes

All changes of the previous releases are included in the latest version.


Version 1.18.0

Important information:

- To update the Schaeffler SmartCheck or ProLink firmware, use always the current version of Schaeffler SmartUtility. 

- Notice for SmartCheck devices: To update a Schaeffler SmartCheck device with firmware version 1.6.30 or prior, 
  first run a update to the version 1.10.0. Only then it is possible to update the Schaeffler SmartCheck firmware 
  to version 1.10.2 or higher!

- Caution! Don’t disconnect the power supply or the Ethernet connection to the Schaeffler SmartCheck or 
  ProLink during firmware update! Otherwise, the process can not be completed and the device is no 
  longer functioning properly.
  
New features:
- The software now also supports the new Schaeffler ProLink system.
- All device data now is stored in one single database. This speeds up the downloading and importing of data.
  Use the "Migrate data" assistant of the SmartUtility full version to convert already downloaded data and 
  transfer them to the database.
- There is now a new plant tree in the SmartUtility Viewer software. Here you can list and arrange 
  your assets and move the measurement jobs from each device to the corresponding asset.
	
Bug fixes:
- [7252] If a configuration contains an alarm map whose cells are not yet filled by the learning mode, 
	the export fails. This has been corrected.
- [7450] In the dialog "Edit device settings" it is now possible to sort by IP address.
- [7594] Information was lost when uploading old belt drive configurations. This has been corrected.
  
Version 1.16.0.25734  
  
New features:
- New communication channels have been added to the Schaeffler SmartCheck device. The Schaeffler SmartUtility 
  software  supports these new communication channels.

Version 1.14.30.25016

New features:
- Data downloads from a Schaeffler SmartCheck device can now be protected with a password.

Bug fixes:
- [6531] The Schaeffler SmartUtility software crashed if the network connection was disrupted while sending
	a configration to a device. This has been corrected.
- [5986] An error was fixed that a user was not notified of a corrupted database during "Analyse data..." 
	This could lead to an empty device list. If there are issues opening a database these are now shown 
	in the device list.	
- [7069] When sending a configuration to the device it was possible that the maximum rotational speed was 
	expressed in RPM instead of Hz. This would lead to a wrong low pass frequency for the configuration. 
	The maximum rotaional speed is now always sent in Hz.
- [5954] If in the Schaeffler SmartUtility software "Analyse data" was selected and the data directory only 
	contains raw data e.g. a download from the Schaeffler SmartCheck or data that originates from a version 1.4 
	or beyond, an empty device list was shown. When clicking on "Next" a message was shown to select a device. 
	Now Schaeffler SmartCheck devices that need have data that needs to be converted to the new format are shown 
	as well, but cannot be selected. These devices have a status icon and a tooltip that give a hint to convert 
	these data prior to a analysis. 
- [7206] If alarm dimensions were defined instead of the standard alarms, it was impossible to 
	export data for these configurations. This was fixed.

Known bugs:
- [7052] The start and end marker for the trends in a report are missing.
  
Version 1.14.0.24149
  
New features:
- The Schaeffler SmartCheck is now able to send data over email. This data can be imported into the
	Schaeffler SmartUtility software as well. The data is divided into a number of small email 
	attachments. One of them is the device config (ending with *.scdc) which is always present. 
	If this file is selected by using the option to import data all data files for that specific 
	device in the same folder are imported. Please note that the email attachments have to be saved 
	into a folder on the computer prior to the import. The Schaeffler SmartUtility contains no function 
	to access the data within your email client.
- The format for the exported data in this software version has been changed. The format is the same that 
	is used in the email attachments of the Schaeffler SmartCheck. The export contains one file 
	for the device config (ending with *.scdc) and one file for each dataset. Since these  
	files are relatively small compared to the prior export function, transport e.g. in an email is 
	tweaked. A further improvement over the previous solution is that these attachments can 
	be imported by the recipient and merged with data already present. That was not possible before.
- DirectX9 as graphic interface for the Schaeffler Viewer software was updated to DirectX11, 
	as DirectX9 is outdated now. Therefore DirectX9 drivers are not installed by the installer anymore. 
- The internal format of the database was changed in comparison with version 1.12.0 of the Schaeffler SmartUtility 
	software. The conversion of an existing database to the new format is performed when a database is 
	accessed and works without user interaction. From then on it is not possible to open the database 
	with an older version of Schaeffler SmartUtility software anymore.	
	
Bug fixes:
- [6531] The Schaeffler SmartUtility software crashed if the network connection was disrupted while sending
	a configration to a device. This has been corrected.
- [5986] It has been fixed that a user was not notified of a corrupted database during "Analyse data...".
	This could lead to an empty device list. If there are issues opening a database these issues are now 
	shown in the device list.	
- [5840] The attempt to copy an empty diagram in the Schaeffler Viewer software to *.rtf-format 
	would lead to a crash of the software. This has been corrected.	

Known bugs:
- [7030] If in the Schaeffler Viewer software the spectrum from a time signal is calculated and the option 
	to display it in a new window is selected the calculated averages and RMS values are wrong. 
	If the calculation is perfomed in the spectrum itself, both values are correct.	
  
Version 1.12.0.23106

New features:
- Japanese translation of the software and all user documentation.  
  
Bug fixes:
- [5144] An error (e.g. because of a blocked or corrupted file) during the rescan of a data directory 
	could lead to an empty result text on the final page of the wizard. This has been fixed.
- [6038] For a Schaeffler SmartCheck that was loaded manually (by the plus button over the device list) in the 
	Schaeffler Viewer it was not possible to show time signals or a spectrum. This has been corrected.
- [6563] For the trends shown in the Schaeffler Viewer no titles were displayed. This has been corrected.

Version 1.10.0.22853
  
New features:
- The Schaeffler Viewer in the Schaeffler SmartUtility software can now display arbitrary bearings with their frequency
	bands in the spectrum viewer. This includes bearings used in measurement configurations and user defined
	bearings. Bearings used frequently can be included in a separate list of favorites.
	
Bug fixes:	
- [5953] In the Schaeffler Viewer software within the list of timesignals a column with rotational speed was shown 
	and all values were 0 RPM. Now the correct values are shown and the user can select between all sources 
	of rotational speed configured per job. 
- [5706] The behaviour that learned alarm levels for the ISO 10816 were set back to the recommendations of 
	the norm has been corrected. Learned alarm levels are preserved until the learning mode is started again.
- [5084] When the alarm limits of a configuration exceeded the recommendations of the ISO 10816, the 
	Schaeffler SmartUtility had set these to the alarm limits of the norm. This has been corrected so that no 
	limits are changed when the alarm limits doesn't stay in the range the norm recommends.
- [5406] Characteristic values for the demodulation signal were not used for the alarm status of a measurement 
	job of type "Used-defined frequency bands". This has been corrected within the Schaeffler SmartCheck. 
	Configurations that are sent with the Schaeffler SmartUtility software to a Schaeffler SmartCheck device are 
	corrected accordingly.
	
Known bugs:
- [6503] If an "Import error" occurs during downloading measurement data in the Schaeffler SmartUtility Viewer, please
	check whether your virus scanner is active. Repeat the process or stop the scan process of the virus scanner 
	until download is complete. This can also occur during importing measurement data.
- [5893] If measurement data was downloaded with a Schaeffler SmartUtility software 1.8.0 and higher, older 
	versions are unable to detect that this data is from a newer version. This will result in displaying just 
	a warning sign in the device tree of the Schaeffler Viewer software without further advice what the reason for 
	this behaviour is.
- [5293] The function "Analyse data" within the Schaeffler SmartUtility will crash with an unhandled exception when 
	the data should be displayed on an additional graphics adapter connected via USB. 
	The workaround is to remove the additional graphics adapter.  
  
Version 1.8.20.20960 

Bug fixes: 	 
- [5792] If the data directory contains raw data from a Schaeffler SmartCheck device smaller version 1.4, these are 
	not shown in the device list of the data analysis. Now these raw data is displayed in the device.
- [5924] When the Schaeffler SmartCheck data contained only trend data without any time signals, it was not possible 
	to import data to the Schaeffler SmartUtility software. Now trends are imported correctly, 
	even if no time signals are present. 
- [5925] In the Schaeffler SmartUtility Viewer software, within the list of time signals a column with rotational 
	speed was shown and all values were 0 RPM. The column was removed as this information is not available yet.

Version 1.8.10.20719

Bug fixes: 	 
- [5886] A firmware update from version 1.4.x to a version 1.6.y will only be possible when the Schaeffler 
	SmartUtility (light) software is started with administrator rights. 
	Now it is possible to perform a firmware update for normal users as well.
- [5431] When updating the firmware of a Schaeffler SmartCheck from version 1.4.x to 1.6.y, the right to delete 
	measurement data from within the Schaeffler SmartWeb was not granted to the administrator user group and 
	could thus not be reinstalled with the Schaeffler SmartWeb. The right is now assigned correctly to the 
	administrator user group.

Version 1.8.0.20540

- In this release, the version number of the Schaeffler SmartUtility (Light) software and the Schaeffler SmartCheck 
  firmware differ. Please note, that the software has the version number 1.8.0, but the accompanying 
  firmware version has 1.6.20. 
  
New features:
- 	 The Schaeffler SmartUtility provides as a new feature template based reports. Reports are generated in the 
	 Rich Text Format (RTF) which is supported by most word processors. Reports can, depending on the template
	 used, contain information about the Schaeffler SmartCheck device along with their alarm status, trends of 
	 measuring jobs and characteristic values and the logbook content of the Schaeffler SmartCheck. Basic 
	 templates are provided but can be widely customized to the needs of the user.
-	 French translation of the software and all user documentation.
	 
Bug fixes: 
- [5564] The Schaeffler SmartUtility software unnecessarily interrupted the measurement process on a Schaeffler SmartCheck 
	 device when the device was manually added and the device information in the software needed to be 
	 refreshed. This has been corrected, the measurement process on the device is now only interrupted 
	 for operations that need additional resources on the device. In any case the measurement process 
	 is started when the operation finishes.
- [5573] When sending a configuration to a Schaeffler SmartCheck device with this software the characteristic value 
	 for triggers and conditions of the source device was transmitted as well. This led to multiple 
	 characteristic values for triggers and conditions on the target device. This bug has been corrected 
	 and the characteristic value is not transmitted any more. 
- [5305] If while sending a configuration or performing a firmware update for a Schaeffler SmartCheck device with 
	 activated user management the authentication failed, the message shown was "No firmware version found" 
	 instead of "Authentication failed". This has been corrected accordingly.
- [5306] If the name of a Schaeffler SmartCheck device was changed using Schaeffler SmartWeb, the new name was not assumed 
	 in the Schaeffler SmartUtility software. This has been corrected.		 
- [5367] After the rescan of a data directory sometimes the device name of a Schaeffler SmartCheck and its IP address 
	 were not displayed. This has been corrected.
- [5589] Schaeffler SmartCheck devices that were manually added could sometimes vanish from the device list in the 
	 Schaeffler SmartUtility making it impossible to download data, perform a firmware update etc. Refreshing 
	 the device list would not always help. Refreshing the device list will not lead to removal of manually 
	 added devices any more.
  
Version 1.6.14.18509  
  
  Bug fixes:
- [5320] The viewer of the Schaeffler SmartUtility would crash when the x-axis was manually changed. The crash 
	 happened when in the trend or the spectrum a couple of signals from different Schaeffler SmartCheck 
	 were selected. This has been fixed.
- [5333] When sending a configuration to a Schaeffler SmartCheck device that was previously downloaded from a 
	 firmware version prior to 1.6.x this configuration was rejected by the Schaeffler SmartCheck if the 
	 alarm values for the ISO 10816 characteristic values were higher than the recommended values 
	 of the ISO 10816. This has been fixed by setting the alarm values to the recommended values 
	 of the ISO 10816 if they are higher.  
  
Version 1.6.12.18250  
  
  Bug fixes:
- [4791] Prior to a firmware update a message is raised saying that measurement data and measurement configuration
	 will be lost due to the firmware update. This is not necessarily true any more. When there are no changes
	 the internal format of a configuration, the measurement configuration is not lost due to a firmware update.
	 The new message reflects this.
- [5157] This software will not overwrite the results of an export. In the past the error message shown when the user
	 attempted an export in a folder where another export of the same Schaeffler SmartCheck existed was "folder already 
	 exits". This did not explain the exact reason. The new message is more verbose. The old export must be 
	 either deleted or moved, or another folder must be selected for the new export.
- [5123] The transmission of a configuration created with a 1.6.10 to a Schaeffler SmartCheck with an firmware version 1.6.6 
	 was completely rejected, although this would only happen if the configuration contains a base configuration. 
	 This has been fixed. Additionally the user gets the hint that he needs to replace the base configuration by 
	 a standard configuration to send the configuration to a Schaeffler SmartCheck with a FW 1.6.6
  
Version 1.6.10.16862  
  
New features:
-	 If sending a configuration to a Schaeffler SmartCheck in which external outputs are defined for an external device 
	 like a PLC these outputs can be selected to be send along with the configuration.
	 
Bug fixes:
- [4900] When the user management on a Schaeffler SmartCheck was active and a firmware update was performed, the user 
	 information on the Schaeffler SmartCheck was overwritten with the default.
- [4870] In "Open devices" the language of the system was submitted in the four letter form. In case of not supported
	 languages the default would be English, even if one of the supplied language would be better suited.
	 e.g. "de-ch" for Switzerland would end up using English even if the supplied language German ("de-de") 
	 would be more appropriate. Now only the two letter code will be used for comparison (in the example above
	 "de" will be used).
- [4861] Logical input channel must have unique names in firmware 1.6.y, whereas these can be non-unique in firmware 
	 1.4.x. In that case, the old configuration could not be send to a Schaeffler SmartCheck 1.6.y. Now the logical 
	 channels with non-unique names will have a number added to their name until it is unique.
- [4801] After updating from SmartUtility 1.4.x to 1.6.y the data directory must be converted to the new format.
	 Attempting to open a data directory that contains only unconverted a correct error message is provided.
- [4788] When external output channels are deleted, the output configuration counter must be resetted.
- [4942] In the Schaeffler SmartWeb 1.4 it was possible to add a second temperature channel for the internal temperature 
	 sensor, with a different scaling factor. Such a configuration is denied by a Schaeffler SmartCheck with firmware 
	 1.6 and higher. Therefore this software tries to change such channels to the default channel internal 
	 temperature.
- [4944] Trend data is not read when the file name including path is too long. The standard path is limited to 260 
	 characters. This can happen on network drives. A error message is now supplied when the path is too long.  
- [4932] The time range in the export will yield an offset to the date depending on the local time zone. The time 
	 range is now correctly converted to UTC, which is internally used.
		 
Known bugs:
- [5025] If a corrupted file of a data download from SmartWeb is about to be imported, the import into the 
	 SmartUtility will fail without a failure notice. Reasons for a corrupted file may be an interrupted data 
	 download.
  
Version 1.6.8.15094  
  
New features:
-	 Alarm limits generated by the learning mode on the Schaeffler SmartCheck device are now always transmitted when a 
	 previously downloaded configuration is sent to the device. Please Note that this applies only to configurations
	 that were downloaded and saved with this version of the software! Previous versions of this software don't 
	 always support the transfer of alarm limits generated by the learning mode.
	 
Bug fixes: 
- [4837] Import of data or rescan data directory lead in some cases to the following error message 
	 "Error while writing AlarmData into database". This was fixed!
- [4813] Sometimes during data download or import it  lead to import errors on Computers with different decimal separator 
	 settings than German. This has been fixed
- [4798] The alarm limits are now stored in the configuration during the download and will be transferred when sending 
	 a configuration.

Version 1.6.2.14695
  
New features:
-	 The data download can be limited to a time interval.
-	 The firmware update to multiple devices can be performed in parallel.
-	 Before commencing a firmware update to a Schaeffler SmartCheck a thorough check is performed, if the update is possible.
-	 A check was added, if the firmware update to a Schaeffler SmartCheck was successful. In previous version only the 
	 successful transfer to the Schaeffler SmartCheck was checked, not the result of the operation on the Schaeffler SmartCheck.
-	 A functionality was added to read data files that were saved previously from SmartWeb.
-	 A data export was added to get data directories of a size that is manageable for e.g. transfer by email. 

Known bugs:
- [4671] The SmartUtility requires the .NET-Framework version 4.5. If on the target system the .NET-Framework version
	 4.5.1 is already present before installing the SmartUtility, the optional .NET language packs are not installed 
	 automatically. Optional means in this case the language packs, that do not match the system language of the underlying
	 Windows. These files can still be installed manually in version 4.5.1.
- [4624] The Schaeffler SmartUtility Viewer has display problems with graphics devices that use the Intel 945 or 965 Chipset. 
	 These drivers are not supported by the manufacturer any more and thus not by the Schaeffler SmartUtility Viewer.

Bug fixes: 
- [4371] When an external source was defined on the Schaeffler SmartCheck the name of the device was not saved,
	 when the configuration of the Schaeffler SmartCheck was downloaded with the data.
- [3616] When configuring the IP address of the Schaeffler SmartCheck, it was possible that the program displayed an
	 error on the result page, even when the operation was successful.
- [3650] Checking the available disk space when saving data fails on network drives.
 
 
Version 1.4.800
  
New features:
-	 Spanish translation of the software and all documentation.
  
Bug fixes:  
  
- [2558] On some computers clicking on one of the links of either the email addresses or the web 
	 address in the about dialog may cause the program to crash.
	 
- [2684] When this release is installed on a computer without uninstalling a previous release
	 first, the entry in Control Panel => Software will be overwritten and thus the previous
	 release cannot be uninstalled over the Control Panel any more. It is still possible to 
	 uninstall by starting "unins000.exe" in the program folder manually.
	 
- [3599] A measuring job with a main alarm will have its alarm level not be updated correctly when the 
	 alarm level of its characteristic would drop from main alarm to pre alarm or no alarm. The overall 
	 alarm status of the Schaeffler SmartCheck will be displayed correctly.
	 
- [3596] Schaeffler SmartCheck with an IP-Address in a different net segment were not found even when the netmask
	 settings were correct.	 

	 
Version 1.4.650  
  
Bug fixes:

- [2973] When downloading a configuration from the Schaeffler SmartCheck it was possible that inactive elements
	 were downloaded along with the active elements. This could result in a configuration that can not
	 be sent to a Schaeffler SmartCheck.

- [3006] Upon creating new identifiers prior to sending a configuration to the Schaeffler SmartCheck, the newly 
	 created identifiers are not guaranteed to be unique. This could result in a loss of configuration
	 elements when the configuration was changed on the device later on.

	 
Version 1.4.512

New features:

- 	 A new viewer program was included. This enlarges Chinese language support to the whole 
	 software package.

- [2292] A new program function was added to convert the old data to the new viewer format.

- [1923] Functionality to check if updates for software and firmware are available was added.
	 This will check in regular intervals and will display a message when a new version is 
	 available. It is recommended to use always the latest firmware version.

Improvements:

- [0824] The standard folder for storing data was changed to c:\data because of the old location was not easily
	 accessible for all users. The folder can still be changed upon the first start of the program.   

- [2445] A manifest was added to the setup program requesting that it is started with administrator
	 privileges.

- [2450] It is now possible to analyse signals concurrently from different devices in the same viewer.

Bug fixes:

- [2291] When Schaeffler SmartCheck were added manually by their IP-address, the device information along with
	 username and password were not saved and thus had to be entered again after each program 
	 start.

- [2426] When two Schaeffler SmartCheck are answering to the broadcast of the Schaeffler SmartUtility at the same moment
	 UDP packets could be lost. This would result in an incomplete list in which not all 
	 devices would be visible.

- [1554] When cancelling a firmware update it was possible for the software to crash.

Known bugs:

- [2682] When this release is installed on a computer without uninstalling a previous release
	 first, the link in the Start Menu will point to the old version. Clicking on it will 
	 start the old version. This can be prevented by creating a link in the Start Menu
	 manually.

- [2835] In the signal properties of a timesignal or a spectrum the number of highest peaks that are 
	displayed can be changed. These can also be marked in the signal by setting the appropriate checkbox.
	The default is 10, the maximum allowed is 1000. On certain graphic cards the viewer software can crash
	if the number of graphical elements gets too high. Therefore it is recommended that the number of 
	highest peaks should not be higher than 50, especially in conjunction with the checkbox that will mark
	peaks from all visible signals.
	
- [3063] If the standard folder for storing data (c:\data by default) contains two folders for the same 
	 Schaeffler SmartCheck the data conversion will only affect one and the other will still be marked as not 
	 converted. This can happen because e.g. one folder was renamed manually and a new folder was created 
	 with the next data download. It is recommended not to change folders in the standard folder manually. 
	 If it is desired to rename a folder it should be moved out of the standard folder instead.

- [3561] Integration results between the Schaeffler Viewer and Schaeffler SmartWeb differ slightly due to different procedures.
	 The SmartWeb uses the filtering of the Schaeffler SmartCheck device, which is not available in the software.