Search term

#WhyWeRace
Simulation technologies in wind power

Simulation technologies in wind power

Schaeffler and Coanda Simsport are partners in the field of sim racing.
Schaeffler and Coanda Simsport are partners in the field of sim racing.

Through its partnership with Coanda Simsport, Schaeffler demonstrates its core expertise in the field of sim racing: In the field of wind power, the global automotive and industrial supplier has been developing innovative and sustainable products and solutions using the latest simulation technologies for many years.

State-of-the-art calculation and simulation programs

Cost-effective wind turbines require reliable components. As one of the world’s leading rolling bearing manufacturers and a development partner to the wind turbine industry, Schaeffler has been producing bearing supports for wind turbines for over 30 years. State-of-the art calculation and simulation programs ensure that optimum designs for components and systems are produced. The entire system is considered, from individual rolling bearings and their components and adjacent construction through to the entire power transmission system, which is displayed and optimized using multi-body simulation programs developed in-house.

Simulation programs provide support in the development of individual bearings through to the design of the entire powertrain.
Simulation programs provide support in the development of individual bearings through to the design of the entire powertrain.

ASTRAIOS large-size bearing test rig

ASTRAIOS simulates real loads and moments that occur in a wind turbine.
ASTRAIOS simulates real loads and moments that occur in a wind turbine.

With its realistic force and moment simulation, Schaeffler’s large-size bearing test rig ASTRAIOS has been providing valuable results, which are used for the new development of bearing solutions and for the optimization of simulation and calculation models.

One of the world’s largest, most modern, and high-performance large-size bearing test rigs enables bearings weighing up to 15 tons and with outside diameters measuring 3.5 meters to be tested under realistic conditions with the aid of a simulation program. ASTRAIOS allows further improvements in the understanding of systems as a whole, influencing factors and the interrelations in the drive trains of wind turbines.

Realistic force and moment simulation

From calm to storm – wind turbines are subjected to constantly changing wind conditions. ASTRAIOS simulates the real loads and moments that occur in a wind turbine.

  • For rotor bearings and slewing rings
  • Testing of all types of rotor bearing supports is possible
  • For wind turbines up to 6 MW

Content Restricted

The following content is restricted due to your privacy settings. In order to view the content, simply activate functional cookies.

I understand, that by activating this option, the previously given data privacy consents will be updated. Read more about our Privacy Policy.

Animation: Simulation of all forces and moments.

Share Page

Schaeffler applies cookies to secure an optimal use. With the further use of this website you accept the application of cookies. More Information

Accept