Search term

Schaeffler makes hydrogen applications more cost-effective – and wins the MATERIALICA Award with its innovative technology

Pressrelease Stage Image
Smiling faces after winning the Materialica Award for Enertect (from left): Robert Metzger, CEO MunichExpo GmbH and award organizer, Dr. Edgar Schulz, expert in the field of coating technologies at Schaeffler, Dr. Mehmet Öte, Director of Coating Technology at Schaeffler, and Laudator Prof. Dr.-Ing. Karl Reiling, Landshut University of Applied Sciences, Professorship in Adhesive Technology and Composite Materials. Photo: Victoria Broome/eMove360°

2023-10-18 | Herzogenaurach/München

  • Steel instead of titanium: Schaeffler Enertect coating range receives MATERIALICA Design + Technology Award 2023
  • Award for sustainable high-performance coating system for metallic bipolar plates with optimized price-performance ratio
  • Schaeffler expands modular coating range for hydrogen technology in fuel cells and PEM electrolysis

With its coating solution Enertect, motion technology company Schaeffler has won the prestigious MATERIALICA Design + Technology Award 2023 in the category “Material”. The Enertect system enables cost-optimized and even more sustainable production of metallic bipolar plates for hydrogen applications. The award was presented at eMove360° Europe 2023, the international trade fair for electric & autonomous mobility, in Munich. Commenting on its decision, the expert judging panel highlighted among other things the up to 99 percent lower carbon footprint of the Schaeffler coatings compared with other coatings available on the market. A total of 8 companies and organizations were nominated as finalists in the categories “Material”, “Product”, “Surface & Technology”, “CO₂ Efficiency”, and “Student”. This is the fifth MATERIALICA Design + Technology Award that Schaeffler has garnered since 2014.

Prof. Dr.-Ing. Tim Hosenfeldt, Senior Vice President Corporate Research and Innovation & Central Technology at Schaeffler, commented as follows: “We are absolutely delighted to have won the MATERIALICA Award once again. Innovative coating solutions like Enertect play a key role in the sustainable mobility of the future, for example in the strategic future growth segment of hydrogen. This award shows that through our intensive R&D activities in surface technology, we are playing an important role towards making hydrogen technology sustainable and viable for the future.”

Enertect: Cheaper and less CO₂ throughout the entire product life cycle
The innovative, high-performance Enertect coating system is used in metallic bipolar plates with proton exchange membrane (PEM) for fuel cells and electrolyzers. The coating maintains a high electrical conductivity over the entire service life of the fuel cells and protects the base material from corrosion. This means that in combination with the coating, less expensive and easily processed steel can be used instead of titanium. The coating, which was developed in-house, is particularly thin and is free of precious metals. Thanks to its special nano-structured design, it is as robust and effective as a solution containing precious metals, but much more sustainable and less expensive. This allows the carbon footprint of the coating to be reduced by more than 90 percent, while the carbon footprint of the entire metallic bipolar plate can be cut by 20 percent. From the beginning of 2024, Schaeffler will start producing bipolar plates with the Enertect PC+ coating in Haguenau in France in the Joint Venture “Innoplate” that it established in partnership with Symbio. Schaeffler is also continuing to develop the product for additional applications.

Publisher: Schaeffler AG
Country: Germany

Related media

Terms of use for Schaeffler press pictures

Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.

We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.

Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.

Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany

presse@schaeffler.com

Downloads

Package (Press release + media)

Share Page

Schaeffler applies cookies to secure an optimal use. With the further use of this website you accept the application of cookies. More Information

Accept