Monitor all assets in a single app Schaeffler OPTIME makes condition monitoring cost-effective for all plant assets

2020-02-12 | Schweinfurt/Hannover
- Schaeffler OPTIME: Comprehensive and automated condition monitoring
- Highly scalable wireless IoT solution
- Easily integrates several hundred assets in a single day
- Cost savings of up to 50 percent compared with manual offline measurement
For cost reasons, permanently installed continuous condition monitoring is typically used only for production machines that are directly process-critical. In the process manufacturing and automation industries, it is therefore not uncommon for up to 95 percent of all assets in a production facility to be either totally unmonitored or monitored only periodically by means of route-based, manual measurements. With Schaeffler OPTIME, however, comprehensive and automated condition monitoring is now a cost-effective proposition for maintenance personnel and facility operators. Schaeffler OPTIME is an efficient and easy-to-use low-cost solution designed specifically for the comprehensive condition monitoring of all indirectly process-critical assets across entire machine and equipment parks.
Automated data analysis powered by Schaeffler expertise
OPTIME is an easily scalable system that consists essentially of wireless, battery-powered vibration sensors, a gateway, and an app to visualize the resulting analysis data. The data captured by the sensors are analyzed using specially developed algorithms that draw on Schaeffler’s technical expertise, its extensive storehouse of physical models developed and refined over many decades, and the experience in condition monitoring that it has built up in the course of its bearing servicing operations. OPTIME provides several weeks’ early warning of damage to machine components such as electric motors, fans, and pumps. It also provides early warning of imbalances, misalignments, and knocking. The app presents trends in graph form and visualizes the severity of incidents using traffic light colors, alarm states, and other information. Assets can be grouped according to users’ requirements, and their condition can be presented in a range of user group-specific views. With OPTIME, in-house maintenance crews and external service contractors receive specific recommendations on the remedial steps required, so they can easily plan their maintenance work, manpower requirements, and spare parts procurement in a timely and cost-efficient manner.
Quick and easy initial operation
OPTIME can be installed and initial operation carried out without any prior condition monitoring expertise, and several hundred measuring points can easily be set up in the space of a single day. The vibration sensors are attached to the monitored assets by means of screws or adhesive, and are activated by the accompanying app, which connects to them via near-field communication (NFC). All installed sensors communicate autonomously with each other and the gateway, thereby forming a dedicated mesh network that ranks among the most reliable and energy-efficient types of IoT networks in use in industry today. The sensors in the mesh network transmit machine KPI data and raw vibration and temperature data via the gateway to the Schaeffler IoT Hub. The hub analyzes the data, and the results are displayed in the app, which supports a very wide range of end devices commonly used by maintenance teams and plant operators. Alternatively, the analysis results can be made available for integration into the customer’s own IT environment via a REST API.
Cost savings of up to 50 percent
OPTIME can yield cost savings of around 50 percent compared with monthly offline measurements made using hand-held devices. It also provides better-quality monitoring than most wireless online CMS systems thanks to its complex, algorithm-based analytics. Moreover, OPTIME can be used for a multitude of assets for which condition monitoring was previously not commercially viable, which makes it the first solution capable of providing an overview of machine states that is truly comprehensive and encompasses all subsystems and auxiliary assets. This is important, because the automated condition monitoring of all assets is fundamental to the reliable prevention of unplanned machine and plant shutdowns.
Publisher: Schaeffler Technologies AG & Co. KG
Country: Germany
Terms of use for Schaeffler press pictures
Schaeffler press pictures may only be used for editorial purposes. Unless otherwise stated, all copyrights and rights of use and exploitation are owned by Schaeffler Technologies AG & Co. KG, Herzogenaurach (Germany) or by one of its affiliated companies. The reproduction and publication of Schaeffler press pictures is only permitted if the source is stated as follows: "Image: Schaeffler". The pictures may be used free of charge in such cases. The use of pictures for advertising or other commercial purposes, in particular their disclosure to third parties for commercial purposes, is hereby prohibited. Pictures may only be edited with the approval of Schaeffler.
We kindly request that a specimen copy be sent to us when Schaeffler press pictures are published in printed media (or a digital copy in the case of publication in electronic media). When using Schaeffler press pictures in films, please notify us and state the title of the film.
Use and utilization of Schaeffler press pictures is subject to the substantive laws of Germany without its conflict of law provisions. The place of competent jurisdiction shall be Nuremberg, Germany.
Postal address:
Schaeffler Technologies AG & Co. KG
Corporate Communication
Industriestrasse 1-3
91074 Herzogenaurach
Germany
Press releases
Package (Press release + media)