Search term

Schaeffler at EMO 2017

At the EMO 2017, Schaeffler presented mechanical components, electric drives, and digitally supported solutions that will ensure considerably more productivity, availability, and quality for the next generation of machine tools - whether it’s for main spindles, feed axes, rotary axes, or rotary tables. One trend is clear – the number of components equipped with sensors in the Schaeffler product range is constantly increasing.

News from the Trade Show Booth

Mechanical Components, Electric Drives, and Digitally Supported Solutions

  • Schaeffler at EMO 2017 – Review

    At the EMO 2017, Schaeffler presented solutions that will ensure more productivity, availability and quality for the next generation of machine tools. The video summarizes the highlights of the week. Finally, CEO Industrial Dr. Stefan Spindler and Ralf Moseberg, Senior Vice President Industrial Automation and Linear Technology, draw a conclusion.

  • Condition Analyses and Forecasts for Machine Components

    Schaeffler introduces a new multi-channel condition monitoring system (CMS) specifically for machine tools: It monitors the condition of several sub-systems of a machine using just a single monitoring system. Sensors from different manufacturers can easily be integrated into the CMS.

    Schaeffler receives 2017 DMG MORI Partner Award

  • Robust, durable and precise – bearing series in X-life quality

    In Hanover, Schaeffler will present a total of four new bearing series in X-life quality. These new X-life bearings offer the machine tool construction sector optimum values in terms of limiting speeds, carrying capacities, as well as rigidity and operating life.

  • Smart components for machine tools

    The driving force behind all new Schaeffler developments is to further increase customer benefit. This is why an increasing number of the company’s purely mechanical products are being integrated into the digital world. A new addition at the EMO 2017 are systems for automatically relubricating linear systems and monitoring main spindle load conditions.

  • EMO 2017 started - Pictures from the start of the show

    At the EMO 2017, Schaeffler is presenting mechanical components, electric drives, and digitally supported solutions that will ensure considerably more productivity, availability, and quality for the next generation of machine tools.

Schaeffler's Highlights

Components and Systems for the Next Generation of Machine Tools

    High-speed spindle bearings in X-life quality: New levels of design freedom for machine tool manufacturers

High-Speed spindle bearings in X-life quality: New levels of design freedom for machine tool manufacturers

Schaeffler will be presenting an entire range of new high-speed spindle bearings in X-life quality at the EMO 2017. These FAG spindle bearings allow machine tool manufacturers to further increase the performance of their motor spindles in terms of mechanical and thermal load carrying capacity and thus offer their customers a boost in both productivity and competitiveness.

Robust spindle drives with innovative Vacrodur rolling bearing material

Vacrodur is an innovative rolling bearing material developed by Schaeffler that allows machine tool manufacturers to significantly increase their spindles’ load carrying capacity and greatly extend their operating life even under extremely difficult conditions. The machine tool manufacturing sector thus benefits from lower unit costs, longer machine running times, and increased availability.

Robust spindle drives with innovative Vacrodur rolling bearing material
Innovations for high-precision rotary tables and rotary axes

Innovations for high-precision rotary tables and rotary axes

Schaeffler offers a highly-specialized modular system that allows customers to select exactly the right components for their rotary tables and rotary axes – that includes high-speed, high-performance, and high-precision designs. Schaeffler will also be presenting new products for this modular system at the EMO 2017: Rotary table bearings with increased performance and extremely smooth-running torque motors.

Requirement-based relubrication is the way to prevent unplanned machine tool downtimes

Defective rolling bearings and linear guidance systems are statistically one of the most frequent causes of machine tool downtimes. Insufficient lubrication or contamination, and in isolated cases even mounting errors are frequently responsible for unplanned linear guidance system failures before the end of the systems’ expected operating life is reached. Requirement-based relubrication for rolling element recirculation guidance systems now allows these unplanned machine downtimes to be drastically reduced and the availability of machine tools to be significantly increased.

Requirement-based relubrication is the way to prevent unplanned machine tool downtimes
Schaeffler integrates sensor technology into its spindle bearings

Schaeffler integrates sensor technology into its spindle bearings

At the EMO 2017, Schaeffler will be presenting a revolutionary system for maximizing the OEE (overall equipment efficiency) of machine tools – a newly developed range of sensors for main spindle monitoring that are integrated into the spindle bearings themselves. For the first time ever, machine manufacturers can now offer their customers a highly effective and easy-to-use instrument for increasing machine availability, productivity, and quality. Using this system will reduce the frequency of spindle failures while simultaneously extending the operating life of the spindles.

Condition analyses and predictions for machine tool components

With a new multi-channel condition monitoring system (CMS) specifically for machine tools, Schaeffler pursues two objectives: Firstly, condition monitoring and condition predictions for various key components in machine tools using a single CMS, and secondly, the flexible integration of sensors from different manufacturers into the CMS.

Condition analyses and predictions for machine tool components
Schaeffler Smart EcoSystem: Added value for machine manufacturers and operators

Schaeffler Smart EcoSystem: Added value for machine manufacturers and operators

What began two years ago with the Machine Tool 4.0 research project has since become a comprehensive infrastructure: The Schaeffler Smart EcoSystem. This allows added value to be generated from the digitalization of machine components.

Linear recirculating ball bearing and guideway assemblies INA KUSE X-life: Load ratings increased by up to 44% and rating life extended approximately threefold

Schaeffler’s INA linear technology proves with its newly-developed, six-row linear recirculating ball bearing and guideway assembly (KUSE) that significant development advances are possible even for well-established products. KUSE X-life assemblies are highly accurate and run extremely quietly, so that they can even be used in measuring machines.

Linear recirculating ball bearing and guideway assemblies INA KUSE X-life: Load ratings increased by up to 44% and rating life extended approximately threefold
Share Page

Schaeffler applies cookies to secure an optimal use. With the further use of this website you accept the application of cookies. More Information

Accept