Search term

Motorsport
FIA World Endurance Championship (WEC)

Hybrid Technology at Schaeffler

Events in Europe, America and Asia, races lasting from six to 24 hours, the participation of renowned manufacturers such as Alpine, Aston Martin, Ferrari, Ford, Porsche and Toyota, divided into four different vehicle classes – the FIA World Endurance Championship (WEC) with the season’s pinnacle event, the legendary 24 Hours of Le Mans, thrills motorsport fans around the globe.

Ideal test laboratory

High Speed und High Tech

The 24 Hours of Le Mans is the world’s major sports car race.
The 24 Hours of Le Mans is the world’s major sports car race.

High speed and high tech – the WEC combines both in special ways, which makes the series an attractive stage on which to demonstrate the innovative power of high-end hybrid sports cars, energy efficiency being the magic word. The 24 Hours of Le Mans in which the drivers spend four times as much time on track as in the other races of the season outshine anything else. Since 2014, the fastest contender in the LMP1 hybrid category has necessarily been the most efficient one as well at Le Mans. The one achieving the longest distance within 24 hours has extracted the maximum from a limited amount of fuel. Due to the considerable technology freedom granted in the areas of hybrid and powertrain technology, the manufacturers keep surprising the audience with ever new innovative impetus.

Schaeffler and Porsche working on forward-thinking technologies in the WEC

For Schaeffler, which performs pioneering work in the development of hybrid systems for production cars, the WEC provides an appropriate environment as well. In 2014, following Porsche’s return to top-flight sports car racing, the company becomes a partner of the premium manufacturer. “The WEC makes the hearts of fans and engineers beat faster,” says Prof. Peter Gutzmer, Deputy CEO and Chief Technology Officer at Schaeffler. “Thanks to the regulations that emphasize efficiency and energy recuperation of the vehicles, there is an active exchange between motorsport and production development.” The Porsche 919 Hybrid is powered by both an IC engine and an electrical system.

Innovative power at Schaeffler and Porsche
Innovative power at Schaeffler and Porsche
Technology transfer as the keyword

Efficiency and reliability. Of crucial importance in the WEC and at Le Mans are exactly the same topics that are in absolute focus of automotive engineering, and thus at Schaeffler, now and will continue to be over the coming decades. The analogy between motorsport and production is again coming very close to its original meaning. Anything that lasts and wins in the world’s toughest races proves its viability for production. In the 24 Hours of Le Mans, revolutionary technologies have passed their baptism of fire and then went on to become firmly established in volume production. In a nutshell, past achievements include streamlined bodywork, lightweight design, disc brakes and hybrid drive systems.

Top-class engineers from Schaeffler and Porsche engaged in exchange
Top-class engineers from Schaeffler and Porsche engaged in exchange
This is how efficiently the Porsche 919 Hybrid operates.
This is how efficiently the Porsche 919 Hybrid operates.
Double world champions three times in succession

The Measure of All Things in the WEC

Following their 2014 debut season, in which Schaeffler and Porsche celebrate their first victory at São Paulo, this corporate pairing soon emerges as the measure of all things in the WEC. Not least thanks to six victories in succession, Timo Bernhard, Brendon Hartley and ex-Formula 1 star Mark Webber crown themselves world champions in 2015. In 2016, Schaeffler and Porsche make their mark in the WEC again. Marc Lieb, Neel Jani and Romain Dumas pull clear of the field with two victories achieved in the first three races and maintain their points-advantage up until the end of the season. The 2017 season goes down in WEC history. Schaeffler and Porsche not only celebrate the drivers’ world championship with Earl Bamber, Timo Bernhard and Brendon Hartley for the third time running but celebrate the title hat-trick in the manufacturers’ classification as well. Schaeffler and Porsche are unbeatable also in each season’s pinnacle event at Le Mans.

From 2015 to 2017 Schaeffler and Porsche dominate the WEC and the 24 Hours of Le Mans.
From 2015 to 2017 Schaeffler and Porsche dominate the WEC and the 24 Hours of Le Mans.
From 2015 to 2017 Schaeffler and Porsche dominate the WEC and the 24 Hours of Le Mans.

From 2015 to 2017 Schaeffler and Porsche dominate the WEC and the 24 Hours of Le Mans.

Success in all three years is guaranteed by the Porsche 919 Hybrid. The sports car prototype combines downsizing turbo technology with efficient gasoline direct injection in a two-liter V4 internal combustion engine. A lithium-ion battery serves as the storage medium for the electrical energy from two different recuperation systems – braking energy from the front axle and exhaust energy. This pioneering technology practically presages the development of powertrain technologies in road-going vehicles, as future consumption and emissions targets can only be fully achieved by electrifying the powertrain. That is why Schaeffler offers numerous solutions and technologies for hybrid systems – from the 48-volt hybrid to the plug-in-hybrid and through to the fully electric vehicle.

Partners in motorsport and production: In 2017, Schaeffler and Porsche won the legendary 24-hour race at Le Mans for the third time in a row.

The championship-winning car 2017: Porsche 919 Hybrid

Looking back on the 2017 championship-winning year, plus Schaeffler and Porsche’s success story in the WEC:

Fact Sheet XXL: WEC 2017

Partners also off the race rack

Intensive and Innovative Partnership – Since as Far Back as 1948

Schaeffler and Porsche are successful not only in the WEC. A flashback to an intensive and innovative partnership between a manufacturer and a supplier with a shared vision of automotive progress: the partnership between Schaeffler and Porsche that started as far back as in the days of the legendary 356 has now been in existence for seven decades. Thanks to cooperation in a spirit of mutual trust, many highlights of automotive progress have been brought to market during this period of time. In addition to hydraulic bucket tappets, they include complex components such as electromechanical camshaft adjusters and roll stabilizers. In 2009, Schaeffler used this technology showcase based on a Porsche Cayenne to demonstrate the optimization potential of modern automobiles yet to be tapped. The wide range of coordinated Schaeffler products used caused fuel consumption and CO2 emissions to drop by ten percent. Schaeffler and Porsche are planning to continue to carry out joint projects in the future – for instance in the field of hybrid and electric powertrains.

Examples from 70 years of partnership

Porsche 356, from 1948

Porsche 356, from 1948

The cage-guided INA needle bearing is a fundamental invention the Schaeffler brothers achieve in the late 40s. Its advantages: reduced friction and torque stability. Many transmissions only become fit for high-speed freeway driving due to these bearings. Obviously, Porsche is among Schaeffler’s customers.

Porsche 911, from 1963

Porsche 911, from 1963

In 1965, Schaeffler founds clutch manufacturer LuK and launches the first diaphragm spring clutch on the European market. This innovation marks the beginning of a successful career. Today, one in three cars around the globe is equipped with a clutch from Schaeffler’s LuK brand.

Porsche 917, 1970

Porsche 917, 1970

In 1970, Porsche evolves from a class to an overall winner at Le Mans. Operating in the twelve-cylinder engine of the 917 are bucket tappets of Schaeffler’s INA brand. For Schaeffler, the racing commitment serves as a test laboratory. Today, Schaeffler has a long history as a specialist in valve train components and systems.

Porsche 928, 1977

Porsche 928, 1977

Schaeffler engineers introduce hydraulics in the valve train. hydraulic bucket tappets like those Porsche puts on the road in the 928 launched in 1977 put an end to time-intensive garage maintenance by the bucket tappets independently adjusting valve lash.

Porsche 959, 1986

Porsche 959, 1986

In the 959 that achieves a speed of over 300 km/h Porsche puts the optimum of what is technically feasible on four driven wheels at the end of the 80s. Among the components on board is the hydraulic chain tensioner, a Schaeffler invention Porsche drivers enjoyed in the 911 as well.

Porsche 911 (Type 996), 1996

Porsche 911 (Type 996), 1996

With VarioCam Plus variable valve control Porsche sets new benchmarks in terms of efficiency and performance. This technology supplied by Schaeffler makes it possible to perfectly adjust engine characteristics to the respective driving mode.

Porsche Cayenne S Hybrid, 2010

Porsche Cayenne S Hybrid, 2010

This Cayenne is the first hybrid vehicle from Porsche. The hybrid module with an integrated electric motor sits between the IC engine and the transmission. A hybrid clutch from LuK harmoniously moderates the interaction between the individual components.

Porsche 918 Spyder, 2013

Porsche 918 Spyder, 2013

The Porsche 918 as a hybrid sports car marks the pinnacle of what is technically feasible. Detailed work and sophistication are featured in abundance here, the wheel bearings from Schaeffler being a case in point. In these bearings, ceramic balls replace the usual steel rolling elements, saving 640 grams of weight.

Videos and Fact Sheets

At a Glance: all Videos and Fact Sheets on the WEC

Share Page

Schaeffler applies cookies to secure an optimal use. With the further use of this website you accept the application of cookies. More Information

Accept