Suchbegriff

Schaeffler at CES 2019 E-Mobility is the Innovation Driver for Schaeffler

Pressrelease Stage Image
Schaeffler’s e-axle serves the requirements of both hybrid and fully electric vehicle powertrains.

07.12.2018 | Herzogenaurach

  • Schaeffler to showcase smart components and system solutions
  • Schaeffler 4ePerformance: all-electric 1,200-hp concept vehicle
  • Customer-focused: hybrid module for American top sellers

Electric mobility is one the key forward-thinking topics at CES 2019. Automotive and industrial supplier Schaeffler predicts that in 2030 some 30 percent of all newly registered passenger cars will be fully electric, 40 percent propelled by hybrid powertrains, in other words a combination of a conventional IC engine and an electric motor, so 70 percent of all passenger cars will be using at least one electric motor as a source of propulsion. At CES, Schaeffler will showcase exhibits extending from a hybrid module through to the 1,200-hp Schaeffler 4ePerformance concept that demonstrate how fascinating and sustainable electric mobility solutions from Schaeffler can be.

E-mobility products from Schaeffler have long made their way into production cars

Alongside digital transformation and IIoT, Schaeffler views electric mobility as an integral component of its forward-thinking “Agenda 4 plus One” program – as one of the key innovation drivers going forward – and has consolidated all of its activities in this field in its new “E-Mobility” business unit. By 2020, Schaeffler will have invested more than 500 million euros in research, development and production of electric drive units. Schaeffler has long begun to mass-produce components and system solutions such as e-axles and hybrid modules. A transmission specifically for electric vehicles of which one each at the front and rear axles of the new Audi e-tron enables a particularly efficient all-wheel drive system with smart control technology is another example. In normal drive mode, only the electric motor on the rear axle is active. If the driver requires higher output via the accelerator pedal or the system detects slip on the rear wheels, the front axle drive is additionally activated.

Schaeffler hybrid module for American top sellers

At CES, Schaeffer will showcase a hybrid module enabling OEMs to electrify the pick-up trucks that enjoy particular popularity in the U.S. marketplace. The compact P2 hybrid module fits between the IC engine and the transmission which makes it suitable for integration into existing vehicle concepts as well. It enables both a boost function and “coasting” with the IC engine shut off as well as all-electric driving. Consequently, the hybrid module shown at CES enhances both fuel economy and driving pleasure.

E-axle for agile handling

The e-axle developed by Schaeffler offers even greater versatility. It can be used either as a stand-alone unit or extend an existing front- or rear-wheel drive into a full-fledged all-wheel drive system. The power output with wheel-selective control is another benefit. Due to torque vectoring, a distribution of torque between the right and left wheels, safety, driving dynamics and ride comfort are noticeably enhanced. Consequently, the e-axle presented at CES offers efficient driving dynamics interventions for hybrid and battery-electric vehicles as well.

Fascinating e-mobility: the Schaeffler 4ePerformance concept vehicle

In the form of the Schaeffler 4ePerformance concept vehicle, Schaeffler has put a particularly fascinating ambassador of electric mobility on wheels that will be another highlight at Schaeffler’s CES booth. The 4ePerformance provides a good example of the technology transfer from racing into a near-production drive concept. The fully electric vehicle uses four Formula E motors with total power output of 880 kW (1,200 hp). They were adopted from the ABT Schaeffler FE01 Formula E race cars and, like the car’s power electronics, developed by Schaeffler’s subsidiary Compact Dynamics. All four motors were used for the full second Formula E season. For Schaeffler, the electric racing series is an ideal test laboratory for the development of electric mobility technologies and ideally fits the company’s “Mobility for tomorrow” strategy with which the globally active technology group helps shape the future of mobility.

Schaeffler benefits from experience in conventional powertrain technology

In the development of electric powertrain components, Schaeffler benefits from the experience the company has gained in conventional powertrains with IC engines, for instance in digital simulation. The know-how from the development of starting elements like the torque converter or the double-clutch broadens the development and manufacturing expertise available at Schaeffler as well. Consequently, combined with its technology expertise, paired with comprehensive systems understanding, Schaeffler is already in a position today to offer its partners fully developed components and system solutions in the field of electric mobility. At the same time, Schaeffler is continually expanding its areas of expertise. Through the acquisition of Elmotec Statomat GmbH, the leading producer of manufacturing machines for mass production of electric motors, Schaeffler is closing the last gap in manufacturing complete electric systems including electric motors produced in-house.


Visit us at CES, Central Plaza, Booth 25.

You will be able to watch the press conference live on January 6th, 2019, at 1:00 pm (GMT-8).

Herausgeber: Schaeffler AG
Ausgabeland: Deutschland

Zugehörige Medien
Downloads

Pressemitteilungen

Paket (Pressemitteilung + Medien)

Seite teilen

Schaeffler verwendet Cookies, um Ihnen eine optimale Nutzung zu gewährleisten. Durch die weitere Nutzung dieser Website stimmen Sie der Verwendung von Cookies zu. Weitere Informationen

Akzeptieren