Publications

Catalogs & Price List

Rolling and Plain Bearings, Price List

 
 
 
 
INA/FAG Price List 2014-07
Catalogue | 2014-05 | English

Price List 2014-07

This price list is valid for deliveries starting 1 July 2014 and supersedes all previous price lists. The Euro prices in this list are valid per piece or per stated unit quantity. The prices do not include VAT. Applicable VAT will be invoiced at the rate specified by law. The prices listed do not constitute a recommended level for onward sale. The catalogue products in this price list represent only a portion of the entire product range. There may be differences in the indication of product designations between the price list, the marking on the bearing itself and the packaging. This price list now contains service products for the mounting, monitoring and maintenance of bearings as well as greases. If products are not included in this list, we will provide prices upon request. This price list is valid for the region of Europe, the Near East, Middle East and Africa. Further information can be found in the foreword to the price list.

Publisher:

 
Catalogue | 2012-08 | 029679141-0000 | English

Rolling bearings (HR1)

Ball bearings, Roller bearings, Needle roller bearings, Track rollers, Bearings for screw drives, Insert bearings/housing units, Bearing housings, Accessories

Catalogue HR 1 stands for pioneering bearing technology, application-focussed advice, the highest product and performance density and continuous development. The benefits to you: - Selection of products from a vast product range; - Maximum benefit, since the most suitable product is used in the right place; - Worldwide product availability; - Short delivery times; - Long term supply capability; - Security of planning for the long view; - Simplified stockholding; - Market-competitive prices; - Global service; - Comprehensive, application-focussed advice.

Publisher:

 
Catalogue | 2009-11 | 036831190-0000 | English

Large Size Bearings (GL1)

Ball bearings Roller bearings Back-up rollers Spherical plain bearings Bearing housings Accessories

Catalogue GL 1 is based on our proven catalogue HR 1, Rolling Bearings. It gives descriptions of standard rolling bearings with an outside diameter of 320 mm or greater and the appropriate accessories as well as numerous special rolling bearings and large plain bearings. We are thus offering an overview of our product range for large and heavy machinery for the original equipment manufacture, distribution and aftermarket sectors. In order to facilitate the selection of suitable products, reference is made at many points to typical applications.

Publisher:

 
Super Precision Bearings Spindle bearings Super precision cylindrical roller bearings Axial angular contact ball bearings
Catalogue | 2011-03 | 036884715-0000 | English

Super Precision Bearings (SP 1)

Spindle bearings Super precision cylindrical roller bearings Axial angular contact ball bearings

FAG super precision bearings for main spindles stand for very high precision and absolute operational security. Innovative FAG spindle bearing solutions are continually raising standards in relation to speeds, accuracy and rating life. For the main spindle system and the overall machine tool system to be successful, however, bearing components alone are no longer sufficient as a guarantee. Significant increases in performance and the creation of unique selling propositions for the customer are now achieved when the bearing manufacturer offers advice and carries out development work on the basis of wide-ranging system knowledge as well as being able to provide support through a range of service functions. It is through close partnership with the manufacturers of spindles and machine tools and through shared knowledge, founded on experience, of the requirements of end users and their customers that the potential exists for achieving a leading role in the market.

Publisher:

 
 
 

Mounting and Maintenance

 
 
 
 
Mounting and Maintenance of Rolling Bearings
Catalogue | 2014-08 | 036908134-0000 | English

Mounting and Maintenance of Rolling Bearings (IS 1)

Products Services Training

This catalogue is aimed principally at maintenance managers and operators of plant in which rolling bearings and other rotating machine components play a critical role in determining the quality of products and processes. Those responsible for maintenance and production processes must be able to rely every day on the quality of their tools and the expertise of their service providers. Through its Industrial Service function, the Schaeffler Group therefore offers high quality products, services and training,

Publisher:

 
 
 

Linear Rolling Bearings and Linear Plain Bearings

 
 
 
 
Driven Linear Units: Linear actuators, Tandem actuators, Clamping actuators, Compact actuators, Telescopic actuators, Linear tables, Drives and contro
Catalogue | 2013-09 | 083780076-0000 | English

Driven Linear Units (AL1)

Linear actuators, Tandem actuators, Clamping actuators, Compact actuators, Telescopic actuators, Linear tables, Drives and controls, Accessories

Rapid progress in the automation of production and assembly processes has pushed forward the development of complete, driven assemblies. These comprise a high precision guidance system, a rigid support rail, a wear-free drive unit with a servo motor and a user-friendly controller. INA linear, tandem and clamping actuators are integrated modular systems containing all the components required for operation. The actuators are guided by linear recirculating ball bearing and guideway assemblies of series KUVE or KUSE or by a track roller guidance system LF. Drive is provided by a ball screw drive KGT or by one or three toothed belts ZR.

Publisher:

 
Catalogue | 2014-01 | 32918356-0000 | English

Track Roller Guidance Systems (LF1)

Track roller guidance systems Track rollers, bolts, guideways Accessories

Track roller guidance systems LF are preferably used, due to their lightweight construction, for tasks in handling systems, where quiet running, high speeds and long travel distances are required together with uniformly low displacement resistance.

Publisher:

 
Catalogue | 2014-02 | 034139060-0000 | English

Shaft Guidance Systems (WF1)

Linear bearings, linear bearing and housing units Solid shafts, hollow shafts Shaft and support rail units Shaft support blocks

Shaft guidance systems comprise shafts or shaft and support rail units combined with low-friction linear ball or plain bearings. The shafts can be either solid or hollow shafts, shaft and support rail units are always solid. For ease of fixing to the adjacent construction, the guidance systems are also available as complete linear bearing and housing units.

Publisher:

 
Catalogue | 2013-12 | 035795131-0000 | English

Monorail Guidance Systems (PF1)

Linear recirculating roller bearing and guideway assemblies Linear recirculating ball bearing and guideway assemblies Linear guidance systems with linear recirculating ball bearing units Accessories

The performance capacity and economic success of a design incorporating monorail guidance systems is essentially dependent on the components used. It is at this stage that the competitive technical superiority and subsequent acceptance in the market of the machine or installation is often decided. However, the bearing arrangement must be precisely matched to the application and achievable by the use of standard components.

Publisher: