Menu

Stories from Schaeffler: Technology and Systems Expertise

Open the Locks for World Trade

The new Panama Canal opened on June 26, 2016. Its locks are so enormous that container ships with a length of 366 meters (1,200 feet) can pass through them. Schaeffler has supplied more than 3,400 bearings for the lock technology and environmentally friendly water management.

The New Panama Canal

The Hunt for Records in Commercial Shipping

13,000 tons of freight and a length of 149 meters (489 feet). When the American steamship “Ancon” was the first to travel on the just completed Panama Canal in 1914, people thought it was huge and it caused debates about whether such large freighters could ever be profitable. 102 years later, a new debut is on the horizon. This first ship to use the new and now third Panama Canal will be the “COSCO Shipping Panama”, a container ship operated by a Chinese shipping company. With a length of 300 meters (984 feet) and a width of nearly 50 meters (164 feet), it can take 400 standard-size containers on board; its maximum load capacity is around 117,000 tons.

The hunt for records in commercial shipping is a direct consequence of growing world trade – and the reason why the Panama Canal has now been expanded to include an additional channel. Until now, passage was only possible for ships that were no wider than 32.3 meters (106 feet). This dimension was so important for international maritime trade that for a long time container ships were built to meet the so-called “Panamax” dimensions. The locks used to be the primary bottleneck: If a ship was built to the maximum width, only 60 centimeters remained between the lock walls and the ocean-going vessel.

Lock Technology

Moving More Than 3,000 Tons

Both on the Atlantic and on the Pacific side, a difference in height of 26 meters (85 feet) must be overcome.
Both on the Atlantic and on the Pacific side, a difference in height of 26 meters (85 feet) must be overcome.

A difference in height must be overcome

After a nine-year construction period, the new, third channel of the Panama Canal opened in the middle of June, allowing ships with a maximum length of 366 meters (984 feet) and a width of around 50 meters (164 feet) to travel this shortcut between the Atlantic and the Pacific Oceans. The new canal will not be able to do without locks either. Both on the Atlantic and on the Pacific side, a difference in height of 26 meters (85 feet) must be overcome first to pass through the interior of the country. This is achieved by three consecutive locks that are flooded with water from adjoining reservoirs.

Enormous gates made of reinforced concrete

The lock gates are made of reinforced concrete and have enormous dimensions: They are 50 meters (164 feet) wide, 30 meters (98 feet) high and 10 meters (33 feet) thick. For safety reasons, two gates have been installed for each barrage that open to the side. To open and close the gate, each has two main drive units that drive a cable winch. Since very high torques of up to 330,000 Nm are required to move the gates, there is also a gearbox on each that increases the torque of the electric motors by almost 280 times. Both at the top and at the bottom of the reservoirs, two so-called “carriages” guide the gates that weigh 3,100 tons. Here guide pulleys are used that must be able to withstand not only the gates‘ dead weight but also the pressure of 430 million liters of water per reservoir. The guide pulleys as well as the gearboxes use bearings made by Schaeffler.

The slow motion of the lock gates causes a quasi-static load in the bearings with very high forces.

Schaeffler engineer Francesco Capittini

Schaeffler engineer Francesco Capittini describes the special challenges as follows: “The slow motion causes a quasi-static load in the bearings with very high forces.” In addition, the operation of the Panama Canal must work reliably 24/7 due to its significance for world trade. Maintenance intervals are scheduled only every five years.

The lock gates are 50 meters (164 feet) wide, 30 meters (98 feet) high and 10 meters (33 feet) thick. (Photo: Panama Canal Authority)
The lock gates are 50 meters (164 feet) wide, 30 meters (98 feet) high and 10 meters (33 feet) thick. (Photo: Panama Canal Authority)
Contribution to Environmental Safety

Reservoirs Provide Resource-saving Water Management

Three reservoirs provide resource-saving water management. (Photo: AFP)
Three reservoirs provide resource-saving water management. (Photo: AFP)

One important feature of the new Panama Canal is its three reservoirs that are located next to each barrage. They ensure that the gigantic expansion project is environmentally friendly. Barrages need a permanent water supply. Until recently, water came mostly from Gatún Lake, a man-made lake created a hundred years ago in the center of the country. The reservoirs, also called “water saving basins” by the operator, provide resource-saving water management. With their help, most of the water is recycled. Several valves open in a channel below ground to drain the water from a barrage. The channel connects the water saving basins and the barrage. Due to the large size of up to seven meters (23 feet), the valves have also been designed as gates. The steel guide pulleys for these gates are also equipped with bearings made by Schaeffler.

International Cooperation

Solutions for Any Case

The construction of the Panama Canal was carried out by highly specialized companies from all over the world. The Italian engineering company Cimolai Technology, for instance, developed the entire mechanism for moving the gates. Matteo Maretto, a member of the development team at the Italian family-owned company, explains: “The bearings are a very critical component for the overall functioning of the lock. They have to work under any circumstances; otherwise the entire facility would stand still. Schaeffler provided valuable support to us during development.” Spherical roller bearings made by Schaeffler are used in the guide pulleys as well as in the drums of the steel cable winches.

The bearings are a very critical component for the overall functioning of the lock. Schaeffler provided valuable support to us during development.

Matteo Maretto, a member of the development team at Cimolai Technology

The gearboxes for the lock gates were developed by PVI Drives, a company of the Brevini Group. The gearbox specialists relied on tapered, spherical and cylindrical roller bearings from Schaeffler. Most of the bearings were specially coated to meet the special operating conditions over a period of 35 years. Hyundai Samho provided the valves that separate the water saving basins and the barrages. Schaeffler supplied the South Korean company with spherical roller bearings for the guide pulleys. The bearings used here are chromium-plated, making them especially resistant to corrosion. When asked about the opening of the new Panama Canal, Dr. Stefan Spindler, who is a member of Schaeffler’s Executive Board and responsible for the company’s industrial business, said: “Our global sales team consists of engineers. They work with Schaeffler experts from a wide range of disciplines, such as coating engineers and calculation experts, which helps them provide our customers with bearing solutions for even the most challenging applications.”

Schaeffler applies cookies to secure an optimal use. With the further use of this website you accept the application of cookies. More Information

Accept