Menu

Stories from Schaeffler: Digitalization

Staying on Track

Flexible maintenance intervals can increase productivity in rail traffic. The technology required for this will be shown by Schaeffler at the 2016 InnoTrans.

Axlebox Bearings

Safety First

The train is rushing along at 300 kilometers per hour. Passengers don’t take much notice; some are reading, others are talking over a cup of coffee in the on-board bistro. The heavy work is carried out by 32 axleboxes that keep the 500-ton train on the track. They not only carry the weight and are subjected to vibrations, but they also have to support the cornering force in every curve. Particularly high loads are applied to the axlebox bearing that functions as the interface between the axlebox and the bogie connected to the car. Axlebox bearings made by Schaeffler are used around the globe in rail vehicles, from subways to high-speed trains.

Axlebox bearings made by Schaeffler are used around the globe, from subways to high-speed trains.
Axlebox bearings made by Schaeffler are used around the globe, from subways to high-speed trains.

Axlebox bearings are components that are important for the safety of every train. That is why they require maintenance on a regular basis.

Dr. Michael Holzapfel, rail expert at Schaeffler

For instance, the axlebox bearings in German ICE trains are replaced after 1.2 million kilometers. Since an ICE travels an average of 1,500 kilometers per day, though, maintenance must be performed after only two years – regardless of the bearing’s technical condition. The axlebox bearings are not disposed of, but rather they are removed, inspected and reconditioned – a time-consuming and expensive process because of the required installation and removal. This brings an obvious idea to mind: Permanently observe the condition of the axlebox bearings during operation and only replace the bearings when they are actually worn, not when you just suspect that they might be. The technology necessary for this, which is called condition monitoring, is the focus of Schaeffler’s trade show presentation at the 2016 InnoTrans.

Condition Monitoring

Longer Maintenance Intervals

As tough as the life of an axlebox bearing may be: If it was made by Schaeffler, it will not show any signs of wear on its mechanical components even after more than a million kilometers – meaning that the axleboxes may be in use longer than the specified maintenance intervals permit. A critical issue is often the lubricant that the axlebox bearing runs in. Shearing forces, pressures and high temperatures all cause the lubricant to age both mechanically and chemically and gradually lose its effect. In extreme cases, the axlebox may overheat – which would result in the immediate decommissioning of the train. How fast this ageing process happens very much depends on the operating conditions.

This is where Schaeffler’s Condition Monitoring System comes in, because in the axlebox bearings, sensors permanently measure the most important loads: speed, temperature and vibration. The data are initially sent to an evaluation unit that is located inside the bogie. This miniature computer constantly calculates the remaining service life of the grease according to a formula developed by Schaeffler experts. This key figure cannot only be represented as plain text on board, but also for the demand-based planning of maintenance intervals.

Someday, big data methods will help us correlate the grease quality and operating conditions from historic data.

Dr. Michael Holzapfel

Such a procedure would allow the forecast capabilities to improve so much that an extension of the maintenance intervals can be achieved regardless of ageing and with the same high level of safety and reliability. In times of increasing traffic, this is a real added value for operators and passengers.

The operator or maintenance technician is connected to the Cloud and can monitor the condition of individual axlebox bearings and even entire axleboxes and bogies.
The operator or maintenance technician is connected to the Cloud and can monitor the condition of individual axlebox bearings and even entire axleboxes and bogies.
Underfloor Drives

Drive Unit Constantly Monitors Itself

Manufacturers of rail vehicles increasingly rely on underfloor drives. Every other wheelset in the ICE 3 is driven by a 500-kilowatt electric motor, allowing trains to do without power cars, which in turn means an increase in transport capacity. At the InnoTrans, Schaeffler will be demonstrating that it is basically possible to expand the Condition Monitoring System from the axlebox bearing to include the complete driven axlebox.

The first prototypes of the new Condition Monitoring System by Schaeffler were first tested successfully in high-speed trains in 2015. Now Schaeffler will be presenting this system to the general public at the 2016 InnoTrans for the first time.
The first prototypes of the new Condition Monitoring System by Schaeffler were first tested successfully in high-speed trains in 2015. Now Schaeffler will be presenting this system to the general public at the 2016 InnoTrans for the first time.

“We are using the same approach that we showed at the Hannover Messe for the machine and plant engineering industry,” said Dr. Holzapfel. As part of a special exhibit on predictive maintenance, Schaeffler presented a drive unit consisting of a motor, gearbox and clutch that constantly monitors itself. Specific functions have now been programmed for use in passenger trains. For instance, the system uses measuring data to detect external influences such as flat spots on the wheel rims that have a negative impact on driving comfort due to their noise development and increase the wear on vehicles and tracks. This type of diagnosis can be displayed as a plain text message in the cab.

The first prototypes of the new Condition Monitoring System by Schaeffler were first tested successfully in high-speed trains in 2015. Now Schaeffler will be presenting this system to the general public at the 2016 InnoTrans for the first time.

Share Page

Schaeffler applies cookies to secure an optimal use. With the further use of this website you accept the application of cookies. More Information

Accept