The eDifferential supports the steering function and has a positive effect on driving dynamics, safety and driving comfort.
The Parallel Hybrid
The overrunning alternator pulley is one of the “unsung heroes”. This inconspicuous component reduces vibrations and improves the energy efficiency of modern engines.
The overrunning alternator pulley
The Serial Hybrid
The lightweight differential
LuK now manufactures more than 100,000 dry dual clutches per month.
The temperature of the motor, turbocharger and transmission as well as the interior can be precisely controlled with the thermal management module.
The rolling bearing supports reduce friction and enable a new balancer shaft design with an optimized mass.
Rotary slide valves controlled by sensors enable the ideal temperature window for the engine and transmission to be reached quickly.
LuK offers both “dry” and “wet” dual clutch solutions.
The innovative thermal management module from Schaeffler reduces fuel consumption and CO2 emissions by up to four percent.
Patín con recirculación de rodillos RUS y guía lineal con jaula plana M/V.
Los nuevos rodamientos para husillos RS de FAG son rodamientos de bolas grandes con un ángulo nominal de contacto de 20 grados y un diseño interior optimizado frente al rozamiento.
High-speed KUVE-B-HS profiled rail linear guides offer speeds of up to 10 meters per second without losses in load carrying capacity and rigidity.
Con los motores torque de segmentos, INA Drives & Mechatronics GmbH & Co. oHG (IDAM) ofrece una elevada rentabilidad. Los motores presentan unas altas velocidades y son muy fáciles de mantener.
The X-life machined needle roller bearing with the Twin Cage: This new combination of cage and rolling elements achieves a significantly lower frictional torque.
Las series de accionamientos RKI de IDAM tienen un par un 30% superior a los motores torque convencionales. La velocidad y la potencia mecánica se han multiplicado por cinco. Al mismo tiempo, la pérdida de potencia se ha reducido hasta un 60 por ciento.
El nuevo rodamiento de rodillos cilíndricos TR térmicamente resistente de FAG combina por primera vez el funcionamiento seguro como rodamiento libre de los rodamientos de rodillos cilíndricos con la aptitud para altas velocidades y diferencias de temperatura variables.
Up to 35 percent less friction – the Schaeffler Group is setting the new standard for deep groove ball bearings with the new FAG Generation C deep groove ball bearing.
Lightweight and compact: The new INA thread guidance roller FRM now has a deep drawn outer ring, which means it is manufactured without cutting. The lower mass provides a considerably improved acceleration capacity.
ACTIVeDRIVE - Electric Vehicle with Active Torque Distribution.
Sistema con recirculación de rodillos RUE para elevadas cargas.
The new FAG high-tech Cronitect hybrid rolling bearing: Increased load carrying capacity, smooth running and reliability.
Flexible: Schaeffler can supply INA compacting roller OWA without a roller covering if required. This enables customers to customize the roller to their own requirements.
Guía hidrostática compacta.
The improved contact between the end face and rib reduces the friction and significantly increases the axial load carrying capacity of cylindrical roller bearings.
Montaje de rodamientos para husillos
The current Schaeffler product range includes more than 400 different overrunning alternator pulleys and more than 140 million of these components have been manufactured in 15 years.
deep groove roller bearing with Lubtect® compound for a reliable supply of lubricant even under critical operating conditions.
Needle roller bearing with Lubtect® compound for a reliable supply of lubricant even under critical operating conditions.
Spherical roller bearing with Lubtect® compound for a reliable supply of lubricant even under critical operating conditions.
In the Schaeffler Hybrid, Schaeffler presents the innovative in-hub motor eWheel Drive. It also allows the development of completely new vehicle architectures.