Schaeffler Australia Pty Ltd

 
 
 
 
The new Black Series Ball Bearing Units from FAG

The new Black Series Ball Bearing Units from FAG stand for easy mounting, quiet running and high reliability.
More information about RIBB

 
PUBLICATIONS
 

Newsletter | 2012-03
Schaeffler Innovation Insight – Issue 1 - 2012

 
Schaeffler Apps

The Technical Pocket Guide (STT) from Schaeffler for your smartphone and tablet
Schaeffler InfoPoint for tablets

Schaeffler Apps

 
Bearing Engineering Services (BES)
Bearing Engineering Services (BES)
 
medias® 5.0
PRODUCT CATALOG

Quickly and easily with our selection assistants:
medias® product selection and information system has been completely revised.

medias 5.0 Product Catalog

 
Stop Fake Bearings
Stop Fake Bearings

Schaeffler takes part in the World Bearing Association's (WBA) campaign launched 2 November. View campaign site at www.stopfakebearings.com

 
PUBLICATIONS
 

Catalogue | 2009-11
Large Size Bearings (GL1)
Ball bearings Roller bearings Back-up rollers Spherical plain bearings Bearing housings Accessories

 
CIVIL ENGINEERING

Bearing supports in buildings and structures are sensitive interfaces, irrespective of whether they are in water or on land. See for yourself how diverse the variety of applications is for Schaeffler rolling bearings and plain bearings in buildings and structures.

Bearing Supports in Buildings and Structures

 
BEARINX®-online Linear Calculation

Efficient Calculation Software by INA/FAG – now available for you, too

BEARINX®-online Linear Calculation

 
MEDIA LIBRARY

The Media Library contains publications, videos and photos about the Schaeffler Group and its products.

Media Library

 

Welcome to Schaeffler Australia and New Zealand

Schaeffler Australia is the center of operations of the Schaeffler Group in Australia and New Zealand for sales, marketing, engineering and logistics for both INA and FAG product brands. The combined standard catalogue contains over 40,000 INA and FAG bearing products.

The unbeatable product range includes needle,cylindrical, spherical, and taper roller bearings, plain bearings, linear systems, slew rings, as well as an extended range of ball bearings and housed units. A full condition monitoring and maintenance product portfolio and bearings reconditioning services is also available to support all your maintenance needs.

Additionally Australia is the ASB Grinding Mill Competence Centre for the group, located in Melbourne; this specialist operation develops solutions for Grinding Mill applications Worldwide.

 

Current messages

2012-02-23 | PRESS RELEASE

Financial Press Conference

In 2011, Schaeffler has significantly exceeded its 2010 record levels of sales and earnings. For the first time in the company’s history, sales topped the €10 billion mark, increasing by 13 percent to approximately €10.7 billion.

more
 
2012-03-19 | LIBRARY

Materials Overview

This publication provides an overview of the range of material solutions that are used in the Schaeffler Group, especially in the Industrial Division, as a widely applied standard or in the form of a specific special solution. The overview serves as an initial reference for business units, sectors, particularly their application engineers and product design departments, external sales, sales functions as well as those interested in getting more intensively involved in the field of materials technology.

TPI 226
 
2012-02-16 | PRESS RELEASE

ASTRAIOS is Prize Winner in the Competition "365 Landmarks in the Land of Ideas"

The ASTRAIOS large-size bearing test rig at Schaeffler’s FAG location in Schweinfurt is a prize winner in the competition “365 landmarks in the land of ideas” and is one of the “locations selected in 2012”. As one of the prize winners in 2012, Schaeffler represents Germany’s capacity to generate innovations in a special way with its new large-size bearing test rig.

more
 
2011-09-15 | LIBRARY

Radial Insert Ball Bearings and Housing Units

The new radial insert ball bearing and housing units FAG Black Series from Schaeffler Group give easy mounting, smooth running and high reliability and thus allow particularly economical bearing arrangements. The dimensions of the FAG housings, made from flake graphite cast iron and with a primer paint coating, conform to JIS B 1559. These single piece cast housings can support moderate to high radial and axial loads. The radial insert ball bearings have basic protection against corrosion due to the Durotect® coating. The bearing units are particularly suitable for applications with moderate to high loads.

Black Series
 
2011-08-01 | PRESS

Schaeffler receives Supplier Award from Porsche for successful cooperation

Schaeffler has been awarded the 2011 Supplier Award by Porsche. The most important components for Porsche’s variable valve control system Porsche VarioCam Plus were among the products praised during the award ceremony.

Outstanding achievements for success
 
2011-05-26 | LIBRARY

Mounting and Maintenance of Rolling Bearings

Those responsible for maintenance and production processes must be able to rely every day on the quality of their tools and the expertise of their service providers. Through its Industrial Service function, the Schaeffler Group offers high quality products, services and training. This catalogue gives an overview of:
- Mechanical Maintenance
- Lubrication
- Condition Monitoring
- Reconditioning
- Maintenance management

Mounting and Maintenance of Rolling Bearings
 
2011-05-24 | LIBRARY

Axial Bearings For high speed main spindles

The bearing arrangement of main spindles in machine tools are subjected to high demands. They must have high load carrying capacity and must at the same time also be suitable for high spindle speeds. Increased load carrying capacity normally brings with it a reduction in the maximum speed. Through the use of the new axial bearings, it is now possible to unify both requirements.

TPI 202
 
2011-05-23 | PRESS

Schaeffler Solutions for Laboratory Automation

When it comes to the subject of “Laboratory Automation”, thinking in complete systems is of prime importance for Schaeffler Group Industrial. This begins with comprehensive engineering support in all stages of the life cycle, so as to create outstanding economical and technical solutions for the customer.

New Design Perspectives Create Customer Value
 
2011-05-23 | LIBRARY

Metal/Polymer Composite Plain Bearings

Metal/polymer composite plain bearings are bearings for very small radial or axial design envelopes. They run with little noise and are particularly suitable where high loads in conjunction with relatively slow rotary and swivel motion must be supported. These products are available as bushes, flanged bushes and thrust washers in two material groups.

Maintenance-free Low-maintenance Special designs, special materials
 
2011-05-23 | LIBRARY

Bearing Solutions for Large Size Machinery

The general trend towards plant with higher productivity is also apparent in larger production systems. As a result, there is increasing demand for correspondingly high performance components and subassemblies of larger dimensions.

TPI 205
 
2011-05-22 | PRESS

Lightweight Differentials Create Space

More compact, lighter, quieter, more efficient and with higher performance – These are the attributes of the new, innovative lightweight differential from Schaeffler's INA brand. This is made possible by a completely new differential design.

Schaeffler innovation revolutionizes the design of differentials
 
2011-05-20 | LIBRARY

FAG Tools for mechanical mounting and dismounting of rolling bearings

Mechanical mounting and dismounting of rolling bearings: Smaller bearings can be driven cold onto the shaft or into the housing for normal tight fits. To prevent bearing damage, the fitting forces must always be applied to the tightly fitted ring. FAG mounting tool sets allow cost-effective and safe mounting of rolling bearings with bore diameters of 10 - 50 mm or outside diameters of 16 - 110 mm. They can also be used to easily mount sleeves, intermediate rings, sales and similar parts. Publisher: Schaeffler Technologies GmbH & Co. KG

TPI WL80-56/2EA