[Skip navigation]

 
Events 

The Schaeffler Group’s Virtual Trade Fair Booth



If you didn’t get the opportunity to visit us at the Hannover Fair, you can now visit our interactive virtual trade fair booth. We are presenting innovations and solutions from our Industrial and Automotive divisions about the leading themes of the fair, namely energy efficiency, total cost of ownership and increasing performance, on various themed "islands".

The following highlights are also being presented:

  • The high-speed linear guidance system KUVE..-B-HS,
  • New bearings in X-life quality such as the new axial spherical roller bearing,
  • The new four-row angular contact ball bearing - "Twin Tandem",
  • Direct drive assemblies from our mechatronics specialist, IDAM,
  • Rolling bearings that also operate without any problems under harsh conditions such as extreme cold or heat, water or acid,
  • The new condition monitoring system called FAG ProCheck, which enables errors to be detected earlier, so that maintenance measures can be planned, thereby considerably reducing overall costs.

The virtual trade fair booth also provides insights into current development projects such as the ball roller bearing that combines the best characteristics of balls and rollers and therefore requires less space.

The Schaeffler Group’s Virtual Trade Fair Booth