FAG’s decades of experience in the development and production of bearings for bicycles are reflected in the new bottom brackets with sensors. E-bikes and pedelecs fitted with these units have a technical advantage and gain greater acceptance in the marketplace. Through precise control and top class smooth running as a result of the “Advanced by FAG” friction optimization, riding enjoyment is increased by a considerable margin.
Publisher: Schaeffler Technologies AG & Co. KG
For over 120 years, FAG has been a world leader in precision rolling bearings. Company founder Friedrich Fischer knew as far back as 1883 that ball bearings are actually synonymous with energy efficiency. After all, the purpose of a ball bearing is to reduce friction, which, in turn, consumes less energy. Consequently, his first bearings were mostly installed – and how could it be otherwise? – in bicycles.
Publisher: Schaeffler Technologies AG & Co. KG
The performance capability and range of e-bikes und pedelecs are determined to a significant extent by the components used. FAG has decades of experience in the development and production of bicycle bottom bracket bearings, which can be seen once again in the sensor bottom bracket bearing BBRS.
Publisher: Schaeffler Technologies AG & Co. KG
The new INA metal-polymer composite plain bearings enable economical solutions in many industrial and automotive applications. They are particularly effective with oscillating movements and achieve a rating life several times higher than that of bearings with conventional materials. In addition, all our new plain bearings are lead-free and, therefore, environmentally friendly.
Publisher: Schaeffler Technologies AG & Co. KG
With our software you can now determine actual stresses while taking shaft deflection and rolling bearing deflection behavior into account. And of course, exact calculations for the internal load distribution in the bearing are performed, including contact pressure with the actual rolling element profile.
Publisher: Schaeffler Technologies AG & Co. KG
Current passage can occur in the use of rolling bearings in: - wheelsets and traction motors (rail vehicles); - direct current and alternating current motors (power transmission); - generators (wind power).
Publisher: Schaeffler Technologies AG & Co. KG
Axial ball bearings and axial cylindrical roller bearings are suitable for supporting high axial loads. However, these bearings should not be loaded in a radial direction and, on account of their cross section, require a relatively large radial installation space in the adjacent construction. Furthermore, single direction designs only support axial loads in one direction. Yet applications frequently call for compact, load-bearing and rigid solutions, which can reliably support combined loads and moments with one bearing arrangement.
Publisher: Schaeffler Technologies AG & Co. KG
Along with developing and manufacturing top quality precision parts, great service is an important tradition at the Schaeffler Group. We offer you the support you need as early as the design phase, so you can put our products into operation with confidence, because for us, service means a partnership with the customer from the first design idea right up to supplying the product.
Publisher: Schaeffler Technologies AG & Co. KG
The main aspects of a bearing that interest skaters are: - How fast is the bearing? - How long will it last? - How does it react to environmental influences? - How heavy is it?
Publisher: Schaeffler Technologies AG & Co. KG
“Rust” is public enemy number 1 for metals. The Schaeffler Group continues to fight back. For example with Corrotect®, an extremely thin, electroplated coating. This gives long term protection of rolling bearings and seal running surfaces against corrosion.
Publisher: Schaeffler Technologies AG & Co. KG